×
Siemens Industry Online Support
Siemens AG
Entry type: Download Entry ID: 26447276, Entry date: 09/06/2007
(0)
Rate

New touchscreen drivers for the 1297, 1597 and 1897 devices

  • Entry
  • Associated product(s)

QUESTION:
Are there new touchscreen drivers for the LCD monitors SCD 1297, SCD 1597 and SCD 1897?

ANSWER:  
The following new touchscreen drivers are available for the above-mentioned devices:

For Microsoft Windows 95 / 98 / 98SE / ME (serial):

EloWin9x_serial.exe ( 396 KB )

For Microsoft Windows 95 / 98 / 98SE / ME (USB):

EloWin9x_usb.exe ( 316 KB )

For Microsoft Windows NT SingleMon (serial):

EloWinNtSingleMon.exe ( 312 KB )

Please note that with this driver you have to calibrate the touchscreen manually. Call the calibration via Control Panel > EloTouch. Calibration is NOT done automatically after a restart.

For Microsoft Windows XP / 2000(serial, USB):

EloWinXP2k.exe ( 1444 KB )

 

Note:
When installing, it is imperative to read the ReadMe files contained in each .exe file. There are different instructions for each operating system.

Keywords:
Elo, Touchtool, Screen driver, LCD monitor

Security information
In order to protect technical infrastructures, systems, machines and networks against cyber threats, it is necessary to implement – and continuously maintain – a holistic, state-of-the-art IT security concept. Siemens’ products and solutions constitute one element of such a concept. For more information about cyber security, please visit
https://www.siemens.com/cybersecurity#Ouraspiration.