×
Siemens Industry Online Support
Siemens AG
Entry type: Download Entry ID: 26574438, Entry date: 10/18/2007
(1)
Rate

Service Pack 3 for SIMATIC iMap STEP 7 Add-On V3.0

  • Entry
  • Associated product(s)


Service Pack 3 (SP3) for SIMATIC iMap STEP 7 Add-On V3.0 has been released for delivery.
The SIMATIC iMap STEP 7 Add-On software package enables STEP 7 users to create PROFINET components without having to install SIMATIC iMap. The SIMATIC iMap STEP 7 Add-On is free of charge and is included on all STEP 7 installation CDs as from STEP 7 version V5.3 SP1 onwards.

 

What’s NEW in Service Pack 3?

In addition to the previously supported operating systems, SIMATIC iMap STEP 7 Add-On V3.0 SP3 now also supports MS Windows Vista 32 Business and Ultimate.

More information on this topic is provided under entry ID 26578762.

 

How can the Service Pack be obtained?

The following options exist to obtain the Service Pack:

  • Download
    As usual, we are offering a free download.
     
  • Service Pack 3 for SIMATIC iMap STEP 7 Add-On V3.0 included on the installation CD of STEP 7 V5.4 SP3
    The SIMATIC iMap STEP 7 Add-On version V3.0 SP3 is included on the installation CD 2 of STEP 7 version V5.4 SP3. This means that all customers with a Software Update Service agreement for STEP 7 will get the SIMATIC iMap STEP 7 Add-On automatically. Furthermore, the iMap STEP 7 Add-on V3.0 SP3 is also part of the download of SP3 for STEP 7 V.4. See entry ID 26578452.
     

Installation prerequisites for the Service Pack:

STEP 7 V5.3 SP3 and higher must be installed.
It is not necessary that an older version of the SIMATIC iMap STEP 7 Add-On is installed.
 

Installation:

  • Start the installation by calling up "SIMATIC_iMap_STEP7_AddOn_V30_SP3.exe"
     

Service Pack 3 for SIMATIC iMap STEP 7 AddOn V3.0
 SIMATIC_iMap_STEP7_AddOn_V30_SP3.exe ( 113335 KB )


Security information
In order to protect technical infrastructures, systems, machines and networks against cyber threats, it is necessary to implement – and continuously maintain – a holistic, state-of-the-art IT security concept. Siemens’ products and solutions constitute one element of such a concept. For more information about cyber security, please visit
https://www.siemens.com/cybersecurity#Ouraspiration.