×
Siemens Industry Online Support
Siemens AG
Entry type: Download Entry ID: 26578452, Entry date: 11/19/2007
(9)
Rate

Service Pack 3.1 for STEP 7 V5.4 and STEP 7 Professional Edition 2006

  • Entry
  • Associated product(s)

DESCRIPTION:

Download of Service Pack 3.1 for STEP 7 V5.4

Installation prerequisites:

  • STEP 7 V5.4 or higher
  • STEP 7 Professional Edition 2006 or higher

Enhancements to the STEP 7 V5.4 Service Pack 3.1 compared to the Service Pack 3:

The setting of the PG/PC interface under the operating systems MS Windows 2000, MS Windows XP and MS Windows 2003 Server is also possible with user rights. Under MS Windows Vista, administrator rights remain a requirement in accordance with the operating system guidelines. 

The archiving program PKZip V8.6 CLI supplied with STEP 7 V5.4 SP3 for the operating systems MS Windows 2000, MS Windows XP and MS Windows 2003 Server is being replaced by PKZip V4.0 familiar from STEP 7 V5.4 SP2. Under MS Windows VistaPKZip V8.6 CLI remains in use. Please observe the notes on the usage in the accompanying product information.   

Options for acquiring STEP 7 V5.4 SP3.1:

Customers that possess a valid Software Update Service agreement (SUS agreement) for STEP 7 will automatically be sent STEP 7 V5.4 incl. SP3.1 on CD-ROM. 

Customers that possess a valid Software Update Service agreement (SUS agreement) for STEP 7 Professional will automatically be sent STEP 7 Professional Edition 2006 Service Release on CD-ROM. This CD contains, among other things, the SP3.1 for STEP 7 V5.4. 

Should you desire to change over to the operating system MS Windows Vista, please note the following information:

  • An operating system update from MS Windows XP to MS Windows Vista is not permissible / possible, if a STEP 7 version has already been installed. Before changing the operating system, it is imperative to deinstall STEP 7 and possibly existing STEP 7 option packages.   
  • Please take note of the changed hardware requirements for STEP 7 under MS Windows Vista described in the ReadMe.rtf file of STEP 7. 
  • If you wish to change over to MS Windows Vista with STEP 7 Professional, the STEP 7 Professional Edition 2006 SR3 or higher is required. It is not sufficient to just install the Service Pack 3 or the Service Pack 3.1 for STEP 7 V5.4.   

 

For customers without SUS agreement, we are offering the following sources: 

  1. Ordering of the CD 
    You can order the Trial License with STEP 7 V5.4 incl. Service Pack 3.1.  
    The order number is: 6ES7810-4CC08-0YA7

    For the current STEP 7 Professional Edition 2006, we are offering the Trial License with the STEP 7 Professional Edition 2006 SR4. This CD with the STEP 7 Professional Edition 2006 Service Release 4 contains, among other things, the SP3.1 for STEP 7 V5.4.      
    The order number is: 6ES7810-5CC10-0YA7

  2. Free Download
    We of course also offer a free download. 

    Caution:
    To avoid an unintentional archiving and possible forwarding of data
    under MS Windows Vista, please be sure to observe the notes of the product information:  

    Product_Information_STEP 7_V54_SP31.pdf ( 50 KB )  

    Furthermore, please observe the following under MS Windows Vista:
    Administrator rights are required for the installation of the STEP 7 software and HSPs, the setup of modules as well as the changing of settings via the application "Set PG/PC interface".

    Service Pack 3.1 for STEP 7 V5.4

    If you already have installed the Service Pack 3 for 
    STEP 7 V5.4, the SP3.1 for STEP 7 V5.4 and for NCM can be installed via the following download:   
    SIMATIC_S7_STEP 7_V54_SP31_alone.zip ( 114294 KB )

    This free download only contains the SP3.1 for STEP 7 V5.4 and for NCM.


    If you have not yet installed the Service Pack 3 for STEP 7 V5.4, you will have to install it first. The SP3 for STEP 7 V5.4 and for NCM can be installed via the following download: 
    SIMATIC_S7_STEP 7_V54_SP3.zip ( 748333 KB )

    This free download contains the SP3 for STEP 7 V5.4 and for NCM.
    This download can be used, if you have previously already installed the following on your PC:  
    STEP 7 V5.4 or
    STEP 7 V5.4 SP1 or
    STEP 7 V5.4 SP2


    Afterwards, please install the SP3.1.

 

Security information
In order to protect technical infrastructures, systems, machines and networks against cyber threats, it is necessary to implement – and continuously maintain – a holistic, state-of-the-art IT security concept. Siemens’ products and solutions constitute one element of such a concept. For more information about cyber security, please visit
https://www.siemens.com/cybersecurity#Ouraspiration.