×
Siemens Industry Online Support
Siemens AG
Entry type: Product note Entry ID: 26578762, Entry date: 10/18/2007
(0)
Rate

Service Pack 3 for SIMATIC iMap STEP 7 AddOn V3.0

  • Entry
  • Associated product(s)

Service Pack 3 (SP3) for SIMATIC iMap STEP 7 Add-On V3.0 has been released for delivery.
The SIMATIC iMap STEP 7 Add-On software package enables STEP 7 users to create PROFINET components without having to install SIMATIC iMap. The SIMATIC iMap STEP 7 Add-On is free of charge and is included on CD 2 of the STEP 7 installation CDs as from STEP 7 version V5.3 SP1 onwards.

What’s NEW in Service Pack 3?

In addition to the previously supported operating systems, SIMATIC iMap STEP 7 Add-On V3.0 SP3 now also supports MS Windows Vista 32 Business and Ultimate.
 

Important notes:

  • It is not possible to update the MS Windows XP operating system to MS Windows Vista, if STEP 7 / STEP 7 AddOn V3.0 SP2 is installed already. Before you change the operating system, please be sure to uninstall STEP 7 / STEP 7 AddOn V3.0 SP2 and possible STEP 7 option packages.
  • To be able to work with MS Windows Vista, you require the SP3 for STEP 7 V5.4. See entry ID 22446648.
  • More information is provided in the readme file


 

How can the Service Pack be obtained?

The following options exist to obtain the Service Pack:

  • Download
    As usual, we are offering a free download. See entry ID 26574438.
     
  • Service Pack 3 for SIMATIC iMap STEP 7 Add-On V3.0 included on the installation CD of STEP 7 V5.4 SP3
    The SIMATIC iMap STEP 7 Add-On version V3.0 SP3 is included on the installation CD 2 of STEP 7 version V5.4 SP3. This means that all customers with a Software Update Service agreement for STEP 7 will get the SIMATIC iMap STEP 7 Add-On automatically. Furthermore, the iMap STEP 7 Addon V3.0 SP3 is also part of the download of SP3 for STEP 7 V.4.
    See entry ID 26578452.
     

Installation prerequisites for the Service Pack:

STEP 7 V5.3 SP3 and higher must be installed.
It is not necessary that an older version of the SIMATIC iMap STEP 7 Add-On is installed.

 

Security information
In order to protect technical infrastructures, systems, machines and networks against cyber threats, it is necessary to implement – and continuously maintain – a holistic, state-of-the-art IT security concept. Siemens’ products and solutions constitute one element of such a concept. For more information about cyber security, please visit
https://www.siemens.com/cybersecurity#Ouraspiration.