×
Siemens Industry Online Support
Siemens AG
文档类型 应用与工具 文档编号 26608353, 文档发布日期 2013年7月9日
(1)
评估

Operation of RFID Systems via Communication Module RF 180C (PROFINET RT) on Windows-based Systems

  • 文档
  • 涉及产品

Task

SIEMENS RFID publications often focus on connecting write/read devices (SLGs) to PLC controllers S7-300/400. The hardware connection is realized via interface modules (ASMs) and the software connection via function blocks. The connection can be made centrally (e.g. via ASM 475, pluggable in S7-300/ ET 200M) or via a bus system (e.g. ASM 456 for PROFIBUS DP-V1 or RF180C for PROFINET IO).

Less familiar, however, is how to connect RFID systems directly to a Windows-based PC by means of connection modules RF 180C via PROFINET IO and how to write on and read from them by means of a C++ application transponder (MDS).

The following picture shows the content of this example.

 
Solution
Using the tools and structures provided by SIMATIC NET you define a "PC station" on your Windows-based system. Using the STEP7 or NCM PC tools, which provide the SIMATIC Manager and the HW Config tool, you configure the software for your hardware configuration. The PC configuration is handled by the station manager. You define your PROFINET IO interface and RFID application via its "Station Component Editor" – comparable with the hardware type plugging of modules in a module rack.

The C++ application which provides an operator user interface for describing and reading the transponder and controls the telegram traffic between PC and ASM, is available as compiled runnable PNIO_RFID.exe file and as open source code. As a user you can use the source program as a basis for your RFID application and adjust it to your individual requirements – appropriate C++ knowledge assumed.

Downloads

Content of Downloads

Download

Dokumentation 26608353_PNIO_RFID_WIN_DOKU_v10_e.pdf ( 1372 KB )
Code
STEP 7 Project, C++-project, Executable Testprogram
26608353_PNIO_RFID_WIN_CODE_v10.zip ( 811 KB )

Last changes
Tested with SIMATIC NET V8.2

安全性信息
为了保护技术基础设施、系统、机器和网络免受网络威胁,有必要实施并持续维护一个全面、最先进的IT安全方案。西门子的产品和解决方案构成了这一方案的一个要素。有关网络安全的更多信息,请访问
https://www.siemens.com/cybersecurity#Ouraspiration.