×
Siemens Industry Online Support
Siemens AG
Entry type: Product note Entry ID: 27045404, Entry date: 11/22/2007
(0)
Rate

SIMATIC Version Cross Manager V7.0 + SP1 Released for Delivery

  • Entry
  • Associated product(s)

Service Pack 1 (SP1) is now available for the SIMATIC Version Cross Manager (VXM) V7.0. In the case of new orders for SIMATIC VXM V7.0 the SP1 will be included in the shipment. Existing SIMATIC VXM V7.0 software can be upgraded under the existing licenses with the SIMATIC VXM V7.0 + SP1 software available for downloading under entry ID 27043127.

Functions/added functions

SIMATIC VXM V7.0 + SP1 can determine the differences between different versions of an engineering project. It can compare complete projects, hardware configurations, CFC/SFC charts, block types and block instances, signals, run sequences, etc. and in this way detect missing, additional or differing objects. It displays the results on a monitor in a combination of tree and tabular representation, which can be printed out or saved as a text file. The differences (objects and attribute values) are marked in color.

As from SP1 the SIMATIC VXM V7.0 has an additional interface that enables the exchange of  engineering data (CAx data) in XML format with design systems.

An overview of the new functions compared to the SIMATIC Version Cross Checker V6.1 is available from the attached "Readme_VXM_V70_SP1.zip" file (VXM-Wasistneu.wri), or in the product-specific online help system under section "What’s new".

Compatibility

SIMATIC VXM V7.0 + SP1 is a 32-bit application for Windows 2000 Professional, Windows XP Professional and Windows Server 2003. To be able to run SIMATIC VXM V7.0 + SP1 you also require SIMATIC STEP 7 V5.3 or higher, or the SIMATIC PCS 7 Engineering Software V7.0 and higher. The full scope of functions of SIMATIC VXM V7.0 + SP1 can only be utilized with the SIMATIC PCS 7 Engineering Software V7.0 + SP1.

More information is available form the readme file which part of the attached "Readme_VXM_V70_SP1.zip" file.

Scope of supply

The SIMATIC VXM V7.0 + SP1 software comes on a TIA Toolset CD, which is supplied together with a License Key Disk and a Certificate of License.

Note: The software is available without the license required for permanent operation on the Toolset DVD of SIMATIC PCS 7 V7.0 + SP1; it can also be downloaded via entry ID 27043127.

Ordering data 

Designation Order No.
SIMATIC Version Cross Manager V7.0 (incl. SP1)
Floating License for 1 user, multilingual (German, English, French, Italian, Spanish), executes under Windows 2000 Professional, Windows XP Professional and Windows Server 2003
Form of supply:
TIA Toolset CD, License Key Disk, Certificate of License
6ES7 658-1CX07-2YA5
SIMATICVersion Cross ManagerUpgradeV7.0  (incl. SP1)
Floating License for 1 user, multilingual (German, English, French, Italian, Spanish), executes under Windows 2000 Professional, Windows XP Professional and Windows Server 2003
Form of supply:
TIA Toolset CD, License Key Disk, Certificate of License
6ES7 658-1CX07-2YE5

 

Installation

Important!
Before beginning with the installation, please read the Product Information leaflet in the readme file (see attached "Readme_VXM_V70_SP1.zip" file).

Readme_VXM_V70_SP1.zip ( 27 KB )
 

Security information
In order to protect technical infrastructures, systems, machines and networks against cyber threats, it is necessary to implement – and continuously maintain – a holistic, state-of-the-art IT security concept. Siemens’ products and solutions constitute one element of such a concept. For more information about cyber security, please visit
https://www.siemens.com/cybersecurity#Ouraspiration.
Rate entry
no rating
Requests and feedback
What do you want to do?
Note: The feedback always relates to the current entry / product. Your message will be forwarded to our technical editors working in the Online Support. In a few days, you will receive a response if your feedback requires one. If we have no further questions, you will not hear from us.