×
Siemens Industry Online Support
Siemens AG
Entry type: Product note Entry ID: 27049176, Entry date: 12/07/2007
(1)
Rate

SIMATIC PDM V6.0 + SP3 Released for Delivery

  • Entry
  • Associated product(s)

Service Pack 3 (SP3) is now available for SIMATIC PDM V6.0. New shipments of SIMATIC PDM V6.0 already include the SP3.

Compatibility

Operating systems:
SIMATIC PDM V6.0 + SP3 will run under the following operating systems:

  • Microsoft Windows 2000 Professional SP3 or SP4
  • Microsoft Windows XP Professional SP2

Integration in SIMATIC PCS 7/SIMATIC STEP 7

SIMATIC PDM V6.0 + SP3 can be operated when integrated in the following configuration environments:

  • PCS 7 V6.1 + SP1
  • PCS 7 V7.0 + SP1
  • STEP 7 V5.2 + SP1
  • STEP 7 V5.3 + SP3
  • STEP7 V5.4 + SP3

Use of the I&M profile of the PROFIBUS user organization and the related use of data set 255 for read and write jobs is only possible with:

  • SIMATIC PDM V6.0 SP3 for stand-alone operation
  • SIMATIC PDM V6.0 SP3, system integrated in SIMATIC PCS 7 V7.0 and higher
  • SIMATIC PDM V6.0 SP3, system integrated in SIMATIC STEP 7 V5.4 and higher

Please note that the included HART OPC Server of the HART Communication Foundation (HCF) has only been released for Windows NT and Windows 2000.

More information is contained in the readme file, which is part of the attached "Readme_PDM_V60_SP3.zip" file below.

Scope of supply:
The SIMATIC PDM V6.0 + SP3 update contains the following CD ROMs:

  • CD 1 with the SIMATIC PDM V6.0 + SP3 software
  • CD 2 with the latest device library (Device Library 2/2007)

Integration and updating of devices
The device library of SIMATIC PDM V6.0 + SP3 (Device Library 2/2007) will integrate new devices and update the device descriptions of existing devices. The HART device library of the HART Communication Foundation (HCF), edition 04/2006, is also involved. More information on the devices listed in the device library of SIMATIC PDM V6.0 SP3 (Device Library 2/2007) is available from the Internet pages of the device manufacturers, as well as from the language-dependent list of devices in the attached "List_of_Devices_2_2007.zip" file.

 List_of_Devices_2_2007.zip ( 1702 KB )
 

The list below provides extracts of some newly included or updated devices (not complete).

 

Device

Classification

Manufacturer

Communication

FCM2000

Sensors - flow - Coriolis

ABB

PROFIBUS PA

FV4000

Sensors - flow - Vortex

ABB

PROFIBUS PA

TZIDC-110

Actuators – electro-pneumatic

ABB

PROFIBUS PA

Prosonic Flow

Sensors - flow - ultrasound

Endress+Hauser

HART

Hach SI792 – SI792C

Sensors - liquids analysis

HACH LANGE

HART

Hach SI792 – SI792D

Sensors - liquids analysis

HACH LANGE

HART

Hach SI792 – SI792E

Sensors - liquids analysis

HACH LANGE

HART

Hach SI792 – SI792P

Sensors - liquids analysis

HACH LANGE

HART

Hach SI792 – SI792T

Sensors - liquids analysis

HACH LANGE

HART

IFC 090

Sensors - flow – electro-magnetic

Krohne

PROFIBUS PA

MFC300

Sensors - flow - Coriolis

Krohne

PROFIBUS PA

MFC300

Sensors - flow - Coriolis

Krohne

PROFIBUS DP

MMI DP Standalone

Sensors - flow - Coriolis

Micro Motion

PROFIBUS DP

MMI DP Step7

Sensors - flow - Coriolis

Micro Motion

PROFIBUS DP

D3

Actuators – electro-pneumatic

PMV

PROFIBUS PA

ET 200M IM Module

Remote I/O

Siemens

PROFIBUS DP

SIMOCODE pro C

Switching device

Siemens

PROFIBUS DP

SIMOCODE pro V

Switching device

Siemens

PROFIBUS DP

SIPART PS2PA

Actuators - electro-pneumatic

Siemens

PROFIBUS PA

SITRANS FUS060

Sensors - flow - ultrasound

Siemens

HART

SITRANS DSIII PROFIsafe

Sensors - pressure

Siemens

PROFIBUS PA

SITRANS TH400

Sensors – temperature

Siemens

PROFIBUS PA

SITRANS TR300

Sensors – temperature

Siemens

HART

SITRANS DA

Sensors – acoustic

Siemens

PROFIBUS DP

IS1 - CPM

Remote I/O

Stahl

PROFIBUS DP

IS1 - Module

Remote I/O

Stahl

PROFIBUS DP

CH420R

Sensors - liquids analysis

Tecfluid

HART

T53.10

Sensors – temperature

Wika

PROFIBUS PA

EJA

Sensors - pressure

Yokogawa

PROFIBUS PA


Installation

Important!
Before proceeding with the installation please read the information of the readme file. It is part of the attached "Readme_PDM_V60_SP3.zip" file.
Existing SIMATIC PDM V6.0 project data will be retained when you update to SP3.

 Readme_PDM_V60_SP3.zip ( 79 KB )

Security information
In order to protect technical infrastructures, systems, machines and networks against cyber threats, it is necessary to implement – and continuously maintain – a holistic, state-of-the-art IT security concept. Siemens’ products and solutions constitute one element of such a concept. For more information about cyber security, please visit
https://www.siemens.com/cybersecurity#Ouraspiration.