×
Siemens Industry Online Support
Siemens AG
Entry type: FAQ Entry ID: 27153767, Entry date: 12/18/2007
(0)
Rate

Which settings do you have to make on the TS Adapter IE to transfer a ProTool project via Teleservice?

  • Entry
  • Associated product(s)

Configuration Notes:
Using the TS Adapter IE (TSA-IE), you can transfer the configuration of a panel or Runtime PC connected to an Ethernet network via the telephone network.

The example below shows the settings to be made on the TS Adapter IE in order to transfer a configuration from your local computer to a panel or Runtime PC.
 

No. Procedure
1 Transfer setting on the TS Adapter IE: 
First, you parameterize the integrated firewall of the TS Adapter IE.
Open the dialog "Options > Administrate TS Adapter IE...".


Fig. 01
2 In the security settings of the TS Adapter IE you must enable the protocols required for the transfer.

Note:
The relevant protocols for incoming and outgoing calls must be enabled.

Below are the settings required for incoming calls.
The settings for outgoing calls are to be made in the same way.

Always save the setting made before you open the next setting mask.


Fig. 02
3 You must enable ICMP (Internet Control Message Protocol) for the Internet protocol. This protocol makes it possible to access IP addresses in the Ethernet network of the TS Adapter IE.

Always save the setting made before you open the next setting mask.


Fig. 03
4 In Expert mode the ports via which the ProTool project is to be transferred must be allowed the firewall of the TS Adapter.

Note:
Normally, the transfer is via Port 2308 or alternatively via Port 50523.

Always save the setting made before you open the next setting mask.


Fig. 04
5 Now make the aforementioned settings for the outgoing calls too.

Finally, the firewall of the TS Adapter IE is configured so that a transfer can be made with ProTool.

Keywords:
Operator panel

Security information
In order to protect technical infrastructures, systems, machines and networks against cyber threats, it is necessary to implement – and continuously maintain – a holistic, state-of-the-art IT security concept. Siemens’ products and solutions constitute one element of such a concept. For more information about cyber security, please visit