×
Siemens Industry Online Support
Siemens AG
Entry type: Download Entry ID: 27202582, Entry date: 08/16/2018
(1)
Rate

Firmware for Siwarex FTA

  • Entry
  • Associated product(s)

Description: 
The firmware can be loaded on the SIWAREX FTA module with software SIWATOOL V4. In addition, two SIWATOOL V4 data base files are included in the .zip-archive. These need to be copied into the SIWATOOL installation folder as described in the information

Release V 9.5.3
 Registrierung notwendig  FTA_FW_9_5_3 (1,6 MB)

This version is mandatory for the current MID certificates (issue date: November 2016)

Change:
 • dosing cycle will not be stopped by an undershooting of -20e

Release V 9.5.2

 Registrierung notwendig  FTA_FW_9_5_2 (1,6 MB)

This version is mandatory for the current MID certificates (issue date: November 2016)

Changes:
• New functions for renewed MID certificates (November 2016)
• Digitale load cells Mettler Toledo: now also PBK9/PFK9-APW can be connected
• General optimizations


Release V 8.5.2

 Registrierung notwendig  FTA_FW_8_5_2 (1,4 MB)

To be used with existing certificates which require this firmware

Changes:
• SecureDisplay (legal-for-trade display together with TIA-Portal) new


Release V 7.4.4

 Registrierung notwendig  FTA_FW_7_4_4 (363,6 KB)

To be used with existing certificates which require this firmware


Release V 5.3.8

  Registrierung notwendig  FTA_FW_5_3_8 (357,2 KB)

To be used with existing certificates which require this firmware

Security information
In order to protect technical infrastructures, systems, machines and networks against cyber threats, it is necessary to implement – and continuously maintain – a holistic, state-of-the-art IT security concept. Siemens’ products and solutions constitute one element of such a concept. For more information about cyber security, please visit
https://www.siemens.com/cybersecurity#Ouraspiration.