×
Siemens Industry Online Support
Siemens AG
Entry type: Download Entry ID: 27774018, Entry date: 04/09/2018
(9)
Rate

Loadable Driver "Modbus Master (RTU)"

  • Entry
  • Associated product(s)
Loadable Driver "Modbus Master (RTU)"
 
Description:

Software requirements
To work with the CP PtP Modbus-Master RTU software  you require the following:

  • An installed version of STEP 7 Basic V5.3 or higher.
  • An installed version of the Point-to-Point Connection Parameter Assignment optional software package ( CP PtP Param ) V5.1 or higher.

The PtP Param software is available for download at entry ID  27013524

Please refer to the STEP 7 Product Information for further software requirements

Hardware requirements

To work with the configuration software of the loadable driver CP PtP Modbus Master RTU  you require the following:

  • Approx. 4 Mbytes of additional memory on your hard drive.
  • Please refer to the STEP 7 Product Information for further hardware requirements
  • The following modules are supported:
    - CP 341
    - CP 441-2
  • The loadable driver CP PtP Modbus Master version V3.1.2 and higher can only be operated on a CP441-2 with order number 6ES7 441-2AA03-0AE0 and higher.

 

Installation
After you have downloaded the current software version you must first unpack the self-extracting Zip archive. After unpacking, start the Setup program by double-clicking the file setup.exe.

 

Overview of the current software versions:

FW
version

Upgrade with ...
  
V3.1 + SP8Recommended for upgrading for STEP7 as of Version 5.6:
For a description, see below V3.1+SP8
 Registrierung notwendig  Modbus-Master318.exe (8,0 MB) 

V3.1 + SP7

Recommended for upgrading for STEP7 < Version 5.6:
For a description, see below V3.1+SP7
 Registrierung notwendig  Modbus-Master317.exe (8,3 MB) 

V3.1 + SP6

For backup only
For a description, see below V3.1+SP6
Modbus-Master316.exe ( 7576 KB )

V3.1 + SP5

For backup only
For a description, see below V3.1+SP5
Modbus-Master315.exe ( 7784 KB )

V3.1 + SP4

For backup only
For a description, see below V3.1+SP4
 Modbus-Master314.exe ( 4488 KB )

V3.1 + SP3

For backup only
For a description, see below V3.1+SP3
Modbus-Master313.exe ( 4096 KB )

V3.1 + SP2

For backup only
For a description, see below V3.1+SP2
Modbus-Master312.exe ( 4056 KB )
  



Loadable Driver Modbus Master (RTU) V3.1+SP8

Together with STEP7 V5.6, the new version V3.1.8 now supports Win10.


Loadable Driver Modbus Master (RTU) V3.1+SP7

The introduction of the SP7 for "Modbus Master (RTU) V3.1" will result in the following additions  / improvements:

  • Can also be installed under Windows 7 / 64 Bit and Windows Server 2008 R2
  • Can also be installed if the option "silent" is used
  • If required, an updated "EDB Component Setup" will also be installed to ensure the correct text representation of diagnostic messages for all STEP 7 versions. 

 

Loadable Driver Modbus Master (RTU) V3.1+SP6

The introduction of the SP6 for "Modbus Master (RTU) V3.1" will result in the following additions  / improvements:

  • Normal operation now also possible in the operating mode half duplex (RS485) two-wire operation
  • Revised online help system (German, English and French)
  • Revised manuals (German, English and French)
  • Revised readmes (German, English and French)

 

Loadable Driver Modbus Master (RTU) V3.1+SP5

The introduction of the SP5 for "Modbus Master (RTU) V3.1" implicates the
following supplements / revisions:

  • Supplement of the baud rate 115200 for CP341-V2 as of edition 1xH02
  • Supplement of the Chinese manuals
  • Revised readmes (German, English and French)
  • Revised manuals (German and English)
  • Revised example Modbus Master 300 (zXX21_05) 

Loadable Driver Modbus Master (RTU) V3.1+SP4

By introducing the SP4 for "Modbus Master (RTU) V3.1" the feature described below has been added:

  • Modbus Master (RTU) V3.1+SP4 can also be installed under Windows VISTA.

 

Loadable Driver Modbus Master (RTU) V3.1+SP3
  • error after receiving incorrect signals in RS485 operation (half duplex) has been corrected
  • error when initializing the RS232 communication has been corrected  
  • error in the "Modbus Master 400" (CP441) sample project has been corrected

 

Loadable Driver Modbus Master (RTU) V3.1+SP2
  • also "outgoing" BREAKs are now entered in the diagnostic buffer
  • after enabling, a diagnostic interrupt is triggered for "incoming" BREAKs
  • Txd and Rxd LED triggering is now compliant with the system (character related)
  • the driver can now be operated with the baud rates of 57.600 bauds (CP341 and CP441) and of 115.200 bauds (CP441)
  • problems with automatic operation of the V24 secondary signals in connection with interrupted transmission path have been corrected
  • the name of the installed example project is now compliant with the system (zXX21_04_PtP_Com_MODMA)
  • in the example project "Modbus Master 300" (CP341) the same value (256) is used for the "LADDR" in HW Config and in OB100.

 

Security information
In order to protect technical infrastructures, systems, machines and networks against cyber threats, it is necessary to implement – and continuously maintain – a holistic, state-of-the-art IT security concept. Siemens’ products and solutions constitute one element of such a concept. For more information about cyber security, please visit
https://www.siemens.com/cybersecurity#Ouraspiration.
Rate entry
no rating
Requests and feedback
What do you want to do?
Note: The feedback always relates to the current entry / product. Your message will be forwarded to our technical editors working in the Online Support. In a few days, you will receive a response if your feedback requires one. If we have no further questions, you will not hear from us.