×
Siemens Industry Online Support
Siemens AG
Entry type: Application example Entry ID: 27833758, Entry date: 10/11/2013
(0)
Rate

Integration of SIMATIC PCS 7 Asset Management into existing projects

  • Entry
  • Associated product(s)
The purpose of this application is to set up the integrated Asset Management into an existing PCS 7 project. The document describes the conditions and the actions required to prepare PCS 7 projects mainly of the versions V5.x and V6.0 for the integration of Asset Management

The following description is based on a server client architecture, in which the Maintenance Server (MS-Server) is configured on a separate PC and the Maintenance Client (MS-Client) is configured on a Engineering Station.

Both, MS-Server and MS-Client are connected to the terminal bus and plant bus.


The document focuses on the following points for the integration of Asset Management:

  • Preparatory activities
  • Engineering and configuring Asset Management

Download

Creation environment

The screenshots have been taken with PCS 7 V7.0 SP1.

Note

Please note the following manuals for the using of SIMATIC PCS 7 Asset Management as of PCS 7 V8.0.

 VersionManual 
 PCS 7 V8.2 SIMATIC Process Control System PCS 7 Maintenance Station 
 PCS 7 V8.1 SIMATIC Process Control System PCS 7 Maintenance Station 
 PCS 7 V8.0 SIMATIC Process Control System PCS 7 Maintenance Station 

 

Security information
In order to protect technical infrastructures, systems, machines and networks against cyber threats, it is necessary to implement – and continuously maintain – a holistic, state-of-the-art IT security concept. Siemens’ products and solutions constitute one element of such a concept. For more information about cyber security, please visit
https://www.siemens.com/cybersecurity#Ouraspiration.