×
Siemens Industry Online Support
Siemens AG
Entry type: Product note Entry ID: 28010740, Entry date: 09/02/2008
(0)
Rate

CP 443-1 Advanced Released for Delivery

  • Entry
  • Associated product(s)
The new SIMATIC NET CP 443-1 Advanced (order no. 6GK7443-1GX20-0XE0) is herewith released for immediate delivery. Initially, the CP 443-1 Advanced will be shipped with hardware release 3 and firmware version V2.0. The new CP 443-1 Advanced (order no. 6GK7443-1GX20-0XE0) succeeds the current CP 44...

The new SIMATIC NET CP 443-1 Advanced (order no. 6GK7443-1GX20-0XE0) is herewith released for immediate delivery. Initially, the CP 443-1 Advanced will be shipped with hardware release 3 and firmware version V2.0.

The new CP 443-1 Advanced (order no. 6GK7443-1GX20-0XE0) succeeds the current CP 443-1 Advanced (order no. 6GK7443-1EX41-0XE0).

 

 

1. Product description

The new CP 443-1 Advanced (order no. 6GK7443-1GX20-0XE0) provides the following new features compared to ist predecessor:

  • Integral Gigabit interface to Gigabit IEEE 802.3ab standards. It is independent of the PROFINET interface and supports Autocrossing, Autonegotiation and Autosensing.
  • Network separation on one module with an additional Gigabit interface
  • Static routing of IP addresses between the Gigabit and the PROFINET interface
  • Higher system availability due to media redundancy in a ring topology by means of the Media Redundancy Protocol (MRP) to IEC 61158 Type 10 "PROFINET" standard
  • Expansion of the IP access list (access to routing and access to the controller can be configured separately)

· Higher performance SEND/RECEIVE blocks (SSEND/SRECV)

  • E-mail with authentification
  • New function block for FTP connection with additional functions
  • For use in H systems (without PN IO function, only ERTEC interface usable)
  • Enhanced Web diagnosis

PROFINET IO controller and PROFINET IO device with support of:

  • RT and IRT realtime feature
  • Enhanced PROFINET IO diagnosis
  • Prioritized startup of PN IO devices

The CP 443-1 Adv (order no. 6GK7443-1GX20-0XE0) is spare part compatible with the CP 443-1 Adv (order no. 6GK7443-1EX41-0XE0)

 

2. Ordering data

 

Product Name

Order No.

CP 443-1 Advanced

 6GK7 443-1GX20-0XE0

 


 

3. Application

The CP 443-1 Advanced is the communication module to connect SIMATIC S7-400 PLCs to Industrial Ethernet. With its own microprocessor the CP unloads the CPU from communication tasks and permits additional connections. The CP 443-1 Advanced provides communication options of the SIMATIC S7-400 PLC with:

· PGs/PCs

· Host computers

· Operator input and control devices

· SIMATIC S5/S7/C7 systems

· PROFINET CBA components

· PROFINET IO devices

PROFINET CBA enables the creation of re-usable technological modules.

User benefits

· Ideally suited for the design of small local networks due to integral 4-port switch; this can save mounting space in a switchboard

· Cost advantage due to network separation  

· High system availability due to support of Media Redundancy (MRP)

· Investment protection for existing systems with the integration of SIMATIC S5 PLCs by means of open communication

· Optimal maintenance support with

Web-based diagnosis

Remote programming via the telephone network (e.g. ISDN) using the WAN feature of TCP/IP  

Monitoring with IT network management tools (SNMP)

Module replacement without PG using the C-PLUG replacement medium (storage also of the file system for IT functions)

· For use in SIMATIC S7-400 H systems (without PN IO function, only ERTEC interface usable)

· Cost-effective access to process information with standard Web-browser; software costs on the client side thus fall away  

· Security: protection against unauthorized access, without change of passwords, with device-specific IP address lists; password protection for Web applications

· System-crossing time synchronization via NTP or SIMATIC procedures with adjustable path selection

· Availability of many subscribers with free UDP connections or Multicast functions

· Easy and fast data exchange of the SIMATIC S7-400 PLCs with field devices via Industrial Ethernet if used as PROFINET IO controller with RT and IRT realtime features  

· Reduction of time and expenses in the design of modular machines and plant with PROFINET CBA

· Easy universal coupling of the PLC to diferent computers via FTP  

· File system as cost-effective bulk memory for data, log files and statistics (C-PLUG as replacement medium)

· Transmission of event-controlled messages via IT communication paths with e-mail (incl. authentification)

· Setting of own IP parameters of series-produced machines without STEP 7

· The socket interface in the partner system can be used without RFC 1006

 

 

4. Miscellaneous:

 

More information on the CP 443-1 Advanced:

 

 

Entry ID

User manual, general section

ID 30374198

User manual, device-specific section

ID 28011203

User manual, Information Technology in SIMATIC S7 with CPs for S7-300 and S7-400

 ID 30565111

Programming manual, functions (FC) and function blocks (FB) for SIMATIC NET S7 CPs

ID 30564821

Programming help, S7Beans / Applets for Advanced CPs

ID 24843906

Version History of IE CPs

ID 56699406 

Program examples

Quick Start CD

 

 

 


Security information
In order to protect technical infrastructures, systems, machines and networks against cyber threats, it is necessary to implement – and continuously maintain – a holistic, state-of-the-art IT security concept. Siemens’ products and solutions constitute one element of such a concept. For more information about cyber security, please visit
https://www.siemens.com/cybersecurity#Ouraspiration.
Rate entry
no rating
Requests and feedback
What do you want to do?
Note: The feedback always relates to the current entry / product. Your message will be forwarded to our technical editors working in the Online Support. In a few days, you will receive a response if your feedback requires one. If we have no further questions, you will not hear from us.