×
Siemens Industry Online Support
Siemens AG
Entry type: Product note Entry ID: 28044589, Entry date: 02/06/2008
(1)
Rate

Release for general availability for Drive ES PCS7 V7.0

  • Entry
  • Associated product(s)
The Drive ES PCS7 V7.0 product is released for sale and general
availability with this information.
The reasons for the revision and further development are the fact that SIMATIC PCS7 V7.0
and V7.0 SP1 have been launched into the market.

Release for general availability: 30th of January 2008

Order Nos. [MLFBs]:

Order No. Product      Availability
6SW1700-7JD00-0AA0 Drive ES PCS7 V7.0, single license     Effective immediately
6SW1700-7JD00-0AA4 Upgrade Drive ES PCS7 V5.x/V6.x to V7.0 for a single license     Effective immediately
6SW1700-0JD00-0AB2 Software update service for
Drive ES PCS7 single license

 

 

Effective immediately
6SW1700-5JD00-1AC0 Runtime license for Drive ES PCS7 Vx.y     Effective immediately

Overview:

  • Compatible to the SIMATIC PCS7 Versions V7.0 and V7.0 SP1
  • Certified with respect to SIMATIC PCS7 V7.0 SP1
     
  • Simulation blocks for the drives have been integrated into the library.
    Simulation blocks are available for the MICROMASTER 4xx, MASTERDRIVES, SIMOREG DC Master and SINAMICS G/S drives
    (incl. ALM and G120).
    These simulation blocks contain a simplified state machine that emulates the real drives. This means that the behavior
    of the faceplates and the block operation on the process side can be simulated, i.e. a test can be made without a real drive actually being physically available.
    The simulation blocks have no know-how protection and can therefore be used in the application as required regarding the simulation - or optimized
    and/or supplemented by system-specific components.
     
  • The"LoopIn_Alarm" function is now supported in conformance with SIMATIC PCS7 V7.0

 

Notes:

·         The blocks can be used for drives after a Y link, if the drives are integrated/linked-in
using a GSD file.
Only PZD communication to control the drives is possible; non-cyclic communication functions to read-out the fault memory are de-activated for operation after the Y link. It is not possible to access drives after the Y link from Drive ES Basic using the engineering tools.

 

Compatibility:

SIMATIC PCS7 V7.0 and V7.0 SP1, Windows XP Prof. and Windows Server 2003
Detailed information regarding the compatibility are provided in ID 18495518

 

How do I obtain the new version?

If you still do not have a version of Drive ES PCS7 then you can order it from new.

Order No.: 6SW1700-7JD00-0AA0

For users that already have a Drive ES PCS7 Version V5.x or V6.x in their possession!

An upgrade version is available. This is provided at a significantly lower price than the full version.
Order No.: 6SW1700-7JD00-0AA4

For those in possession of the Software Update Service 6SW1700-0JD00-0AB2!
Customers in possession of a Software Update Service will automatically receive the new version.
More detailed information regarding managing the Software Update Service is provided in ID 13532008

 

Availability of previous versions:
The existing versions of Drive ES PCS7 Versions V5.1, V5.2, V6.0 and Version V6.1 are still available - for
compatibility reasons - to the corresponding SIMATIC PCS7 Versions V5.1, V5.2, V6.0 and V6.1.

 

The single license is the engineering license that must be purchased for each engineering station - and that is already known. The engineering license also automatically includes a runtime license that authorizes customers/users to download the software to an AS station. Additional runtime licenses must be purchased for additional AS stations.

The upgrade version for Drive ES PCS7 from V5.X and V6.x to V7.0 is intended for those customers that already have one or several licenses in their possession.
Customers are able obtain the new version at a significantly lower price.
Caution! The upgrade checks whether the previous version is installed and only then can the new version be installed.

The update service brings customers into a position so that they are supplied automatically with all of the service packs and full versions for one year. The customer then always has the up-to-date software. This service will be invoiced.
Note! Users that have ordered the update service will automatically receive the new version.

The runtime license for Drive ES PCS7 V7.0
When this license is purchased (it comprises a software certificate with license and adhesive label) then the user is licensed to download our blocks and use them on 1 AS station. As proof that the runtime license has been purchased the label supplied can be glued onto the AS station or in the appropriate documentation ( e.g. machine logbook ).

Security information
In order to protect technical infrastructures, systems, machines and networks against cyber threats, it is necessary to implement – and continuously maintain – a holistic, state-of-the-art IT security concept. Siemens’ products and solutions constitute one element of such a concept. For more information about cyber security, please visit
https://www.siemens.com/cybersecurity#Ouraspiration.
Rate entry
Requests and feedback
What do you want to do?
Note: The feedback always relates to the current entry / product. Your message will be forwarded to our technical editors working in the Online Support. In a few days, you will receive a response if your feedback requires one. If we have no further questions, you will not hear from us.