×
Siemens Industry Online Support
Siemens AG
Entry type: Download Entry ID: 28056407, Entry date: 12/05/2011
(0)
Rate

BIOS-Download for SIMATIC Box PC 827B

  • Entry
  • Associated product(s)

The BIOS updates each contain the changes of the earlier versions listed in the info texts.

Please pay careful attention to the following points before or when installing the BIOS update

  • Use the most recent version possible of the BIOS (current release version). Using an older BIOS on a new PC platform can lead to faults.
  • The USB stick or USB disk drive must be the first drive in the boot sequence.
  • Make sure that the power supply is not cut off.
  • Under no circumstances whatsoever should you switch off the device during the update process.
  • Under no circumstances whatsoever should you interrupt the update procedure.

If you do not comply with the points above, you might cause irreparable damage to your PC!

Note
How to perform a BIOS update is explained in the "Update.txt" file in the ZIP file.



Following the BIOS update, the system must be brought into a defined basic state. Proceed as follows to do this:

  • Start the BIOS Setup with the F2 key.
  • Load the BIOS default configuration with the F9 key (Setup Defaults) or via the BIOS Setup command "Get Default Values" in the Exit mask.
  • Save the settings using the BIOS Setup command "Save Change & Exit" or with the F10 key "Save configuration changes and exit".
BIOS for SIMATIC Box PC 827B
Version
V110204
V110204_Info.txt ( 3 KB )  
Version
V110205
V110205_Info.txt ( 3 KB )  
Version
V110206
V110206_Info.txt ( 4 KB )  
Version
V110207
 V110207_Info.txt ( 5 KB )  
Version
V110208
V110208_Info.txt ( 6 KB ) Current release version

Please contact Technical Support as below to receive the BIOS update:

Support Request
http://www.siemens.com/automation/support-request

Internet
http://support.automation.siemens.com

Additional information
A list of the current driver versions is available in Entry ID: 51339179.

Security information
In order to protect technical infrastructures, systems, machines and networks against cyber threats, it is necessary to implement – and continuously maintain – a holistic, state-of-the-art IT security concept. Siemens’ products and solutions constitute one element of such a concept. For more information about cyber security, please visit
https://www.siemens.com/cybersecurity#Ouraspiration.