×
Siemens Industry Online Support
Siemens AG
Entry type: Product note, Entry ID: 28368485, Entry date: 02/11/2008
(1)
Rate

Delivery release: SIMOCODE ES 2007 for SIMOCODE pro

  • Entry
  • Associated product(s)

SIMOCODE ES 2007 is the central software for the commissioning, operation and diagnostics of SIMOCODE pro 3UF7. Delivery release of the software has been granted as per February 2008.










SIMOCODE ES 2007 is the central software for the commissioning, operation and diagnostics of SIMOCODE pro 3UF7. The new SIMOCODE ES 2007 offers the following essential innovations:
 
1. New license model:
With conversion to SIMOCODE ES 2007, also the A&D-uniform license management system "Automation License Manager“ is employed. This facilitates an advance testing of the software's full functional scope (Premium package) over a 14-day free trial license period. With the floating license, only the actually used license is paid for, thanks to which the software can be installed as often as required. Licenses can be rapidly downloaded from the Mall.
 
2. New functions:
As functional expansion, particularly the new typical files should be pointed out. They facilitate the creation of parameter typicals for identical motor starter times with many similar parameters. Via the export function for parameters in a text file, these values are externally provided for further processing. Furthermore, the parameters' print-out now complies with documentation in accordance with DIN EN ISO 7200. As further novelty, access to SIMOCODE pro with teleservice via MPI is supported.
 
3. New software versions:
SIMOCODE ES 2007 is offered in 3 product versions:
 
  • Basic version
  • Standard version
  • Premium version
 
4. New order numbers:
 
SIMOCODE ES 2007 PREMIUM, 3ZS1 312-6CC10-0YA5
FLOATING LICENSE F. ONE USER, E-SW   
SIMOCODE ES 2007 PREMIUM, 3ZS1 312-6CE10-0YB5 
FLOATING LICENSE F. ONE USER, E-SW,
LICENSE KEY DOWNLOAD
 
SIMOCODE ES 2007 PREMIUM, 3ZS1 312-6CC10-0YE5 
UPGRADE F. SIMOCODE ES 2004 OR HIGHER  
SIMOCODE ES 2007 PREMIUM, 3ZS1 312-6CC10-0YD5
POWERPACK F. SIMOCODE ES 2007 STANDARD  
SIMOCODE ES 2007 PREMIUM, 3ZS1 312-6CC10-0YL5
SOFTWARE UPDATE SERVICE  
 
SIMOCODE ES 2007 STANDARD, 3ZS1 312-5CC10-0YA5
FLOATING LICENSE F. ONE USER, E-SW   
SIMOCODE ES 2007 STANDARD, 3ZS1 312-5CE10-0YB5
FLOATING LICENSE F. ONE USER, E-SW, 
LICENSE KEY DOWNLOAD
 
SIMOCODE ES 2007 STANDARD, 3ZS1 312-5CC10-0YE5
UPGRADE F. SIMOCODE ES 2004 OR HIGHER  
SIMOCODE ES 2007 STANDARD, 3ZS1 312-5CC10-0YD5
POWERPACK F. SIMOCODE ES 2007 BASIC  
SIMOCODE ES 2007 STANDARD, 3ZS1 312-5CC10-0YL5
SOFTWARE UPDATE SERVICE  
 
SIMOCODE ES 2007 BASIC, 3ZS1 312-4CC10-0YA5
FLOATING LICENSE F. ONE USER, E-SW   
SIMOCODE ES 2007 BASIC, 3ZS1 312-4CE10-0YB5
FLOATING LICENSE F. ONE USER, E-SW, 
LICENSE KEY DOWNLOAD
 
 
Further information and the corresponding product brochure will soon be available in the A&D Mall or at:
 


Downloads
Brochure_SIMOCODE_ES ( 322 KB )


Security information
In order to protect plants, systems, machines and networks against cyber threats, it is necessary to implement – and continuously maintain – a holistic, state-of-the-art industrial security concept. Siemens’ products and solutions constitute one element of such a concept. For more information about industrial security, please visit
http://www.siemens.com/industrialsecurity.