×
Siemens Industry Online Support
Siemens AG
Entry type: Application example Entry ID: 28430682, Entry date: 04/10/2015
(1)
Rate

Configuration of Redundant I/O Modules in SIMATIC PCS 7

  • Entry
  • Associated product(s)
In principle, the high availability in PCS 7 can be used at all levels. With SIMATIC ET 200M modules, the distributed I/O can also be designed as redundant.

In this documentation the emphasis is placed on the application of redundant distributed I/O using ET 200M modules. Thereby, particularly the wiring options of the input/output modules as well as the individual configuration steps are explained.

Main contents
The document focuses on the following points:

  • Redundant I/O modules especially with channel granular functionality
  • Setup, wiring and configuration of redundant ET 200M stations
  • Using Marshalled Termination Assemblies (MTA) as an interface between the distributed I/O modules and the acutators or sensors
  • Diagnostics options on a fault-tolerant system with redundant I/Os in case of an error

Validity
SIMATIC PCS 7 V8.1, V8.0, V7.1, V7.0

Documentation
 Configuration of Redundant I/O Modules in SIMATIC PCS 7 (From PCS 7 V8.1)
 Configuration of Redundant I/O Modules in SIMATIC PCS 7 (From PCS 7 V7.0 SP1)

Last Changes
Update for SIMATIC PCS 7 V8.1

 

Security information
In order to protect technical infrastructures, systems, machines and networks against cyber threats, it is necessary to implement – and continuously maintain – a holistic, state-of-the-art IT security concept. Siemens’ products and solutions constitute one element of such a concept. For more information about cyber security, please visit
http://www.siemens.com/industrialsecurity.