Entry type: FAQ, Entry ID: 2907670, Entry date: 08/25/2000

Two-line messages with S7-PDIAG and OP27/TP27

  • Entry
  • Associated product(s)

How can you configure two-line messages in S7-PDIAG?

When configuring message texts in S7-PDIAG, the formatting character "\n", known from ANSI C, is inserted at the point in the text where the line break is supposed to be. The line break is also displayed correctly in the "CPU messages" window.