×
Siemens Industry Online Support
Siemens AG
Entry type: Application example Entry ID: 29088810, Entry date: 04/25/2008
(0)
Rate

Audible Alarms for PCS 7 Web Clients

  • Entry
  • Associated product(s)
This applicative solution has been created in response to customer needs for audible alarms on the PCS 7 Web clients.

Objective of the application

This applicative solution has been created in response to customer needs for audible alarms on the PCS 7 Web clients. Audible alarms are a feature of the PCS 7 OS environment but are not available to the Web clients as a standard feature.

Main contents

This application deals with the following key elements:

  • Ready-made C-scripts for downloading and implementation (e.g. Windows API called on the Web client to produce sounds)
  • Step-by-step configuration instructions

Note
If the option "Use horn on Web client" is available in the properties of the user in PCS 7 OS User Administration, then this solution is not needed.

Validity

This application is valid starting from PCS 7 V7.0 SP1.

Downloads

Content of Downloads

Download

Audible Alarms for PCS 7 Web Clients 29088810_Audible_Alarms_WebClient_en.pdf ( 1794 KB )
Code
Global action "SoundCycle.pas" and project function "Sound.fct"
29088810_Code.zip ( 1 KB )

 

History

Version

Modification

04/2008 First release

 

Security information
In order to protect technical infrastructures, systems, machines and networks against cyber threats, it is necessary to implement – and continuously maintain – a holistic, state-of-the-art IT security concept. Siemens’ products and solutions constitute one element of such a concept. For more information about cyber security, please visit
https://www.siemens.com/cybersecurity#Ouraspiration.