×
Siemens Industry Online Support
Siemens AG
Entry type: Product note Entry ID: 29746989, Entry date: 09/10/2008
(1)
Rate

STEP 7 Professional 2006 Service Release 5

  • Entry
  • Associated product(s)

The current product DVD of the STEP 7 Professional Edition 2006 has been updated with the Service Pack 4 (SP4) for STEP 7 V5.4, the Service Pack 5 for S7-SCL V5.3, the Service Pack 6 for S7-GRAPH V5.3 and with the Service Pack 2 of S7-PLCSIM V5.4. It is now available for ordering. Customers with a valid Software Update Service agreement for STEP 7 Professional will receive the DVD with the STEP 7 Professional Edition 2006 Service Release 5 automatically.

Customers without a Software Update Service agreement for STEP 7 Professional can order the Trial License with STEP 7 Professional Edition 2006 Service Release 5 under the order no.: 6ES7810-5CC10-0YA7. Alternatively, you can also install the Service Packs of the individual products on the existing STEP 7 Professional Edition 2006, e.g. the SP4 for STEP 7 V5.4 via DVD or download (see entry ID 29753195 ).

Prerequisites for the installation of STEP 7 Professional Edition 2006 Service Release 5:

  • STEP 7 Professional Edition 2006

Supported operating systems:

  • MS Windows XP Professional  SP2
  • MS Windows Server 2003 SP2 standard edition with or without R2 as workstation computer
  • MS Windows Vista 32-bit Ultimate and Business
     

Important:

  • It is not possible to update the MS Windows XP operating system to MS Windows Vista, if STEP 7 Professional is installed already. Before you change the operating system, you should be sure to uninstall STEP 7 Professional and possible STEP 7 option packages.
  • If you wish to change to MS Windows Vista with STEP 7 Professional, you require the STEP 7 Professional Edition 2006 SR3, SR4 or SR5.
    It is not sufficient to only install Service Pack 4 for STEP 7 V5.4.
  • More information is available from the readme files

Important for the operating systems:

  • With the STEP 7 Professional Edition 2006 SR5, the Microsoft Internet Explorer version 6.0 or higher is mandatory for all operating systems. 

What’s NEW?

As from STEP 7 Professional Edition 2006 Service Release 2 the software is supplied on DVD and the license on a USB stick.

Service Release 5 of the STEP 7 Professional Edition 2006 includes updates of the following software:

  • STEP 7 V5.4 incl. SP4
  • S7-SCL V5.3  incl. SP5
  • S7-GRAPH V5.3 incl. SP6
  • S7-PLCSIM V5.4 incl. SP2

Ever since the new licensing concept for STEP 7 Professional 2004, we are also offering a cost-effective Trial License for validation purposes (not for productive use). This DVD enables you to test all the software packages contained on it for 14 days (from the day of first starting the software). Thereafter, the complete software can be enabled for an unlimited period with the Floating License of STEP 7 Professional, without the need for post-installation.  

The Trial License for STEP 7 Professional replaces the previous Presales Package.

Ordering data for the STEP 7 Professional Edition 2006 SR5 Trial License:

Order No.

Designation

6ES7810-5CC10-0YA7

SIMATIC S7, STEP7 PROFESSIONAL 2006 SERVICE RELEASE 5
DATA CARRIER INCL.TRIAL LICENSE

 

Security information
In order to protect technical infrastructures, systems, machines and networks against cyber threats, it is necessary to implement – and continuously maintain – a holistic, state-of-the-art IT security concept. Siemens’ products and solutions constitute one element of such a concept. For more information about cyber security, please visit
https://www.siemens.com/cybersecurity#Ouraspiration.