×
Siemens Industry Online Support
Siemens AG
Entry type: Download, Entry ID: 29753195, Entry date: 11/17/2008
(2)
Rate

Service Pack 4 for STEP 7 V5.4 and STEP 7 Professional Edition 2006

  • Entry
  • Associated product(s)

DESCRIPTION:

Download of Service Pack 4 for STEP 7 V5.4 

Prerequisitesfor installation:

  • STEP 7 V5.4 or
  • STEP 7 Professional Edition 2006 

Please also read the information (What’s NEW, special hints, etc.) which we have compiled for you in entry ID 29753194.

Customers with a valid Software Update Service agreement for STEP 7 will receive the DVD with STEP 7 V5.4 incl. SP4 automatically.

Customers with a valid Software Update Service agreement for STEP 7 Professional will receive the DVD with the STEP 7 Professional Edition 2006 Service Release 5 automatically. The SP4 for STEP 7 V5.4 is part of this Professional DVD (see entry ID !29746989! ).

If you wish to change to the Windows Vista operating system, please note the following:

  • It is not possible to update the MS Windows XP operating system to MS Windows Vista, if STEP 7 is installed already. Before you change the operating system, please be sure to uninstall STEP 7 and possible STEP 7 option packages.
  • Please also note the different hardware requirements in the case of STEP 7 with MS Windows Vista as described in the readme.rtf file of STEP 7.
  • If you wish to change to MS Windows Vista with STEP 7 Professional, you require the STEP 7 Professional Edition 2006 SR3, SR4 or SR5.
    It is not sufficient to only install Service Pack 4 for STEP 7 V5.4.

 

Customers without Software Update Service agreement can obtain the SP4 as follows:

  1. DVD:  You can order the Trial License with STEP 7 V5.4 incl. Service Pack 4 on DVD. The order no. is: 6ES7810-4CC08-0YA7

    For the current STEP 7 Professional Edition 2006 you can obtain a Trial License with the STEP 7 Professional Edition 2006 SR5.
    The DVD with the STEP 7 Professional Edition 2006 Service Release 5 also includes the SP4 for STEP 7 V5.4
    The order no. is: 6ES7810-5CC10-0YA7
  2. Free Download
    As usual, we are offering a free download.


    Service Pack 4 for STEP 7 V5.4
    SIMATIC_S7_STEP7_V54_SP4.zip ( 792360 KB )  

    This free download includes the SP4 for STEP 7 V5.4 and NCM and can only be installed, if STEP 7 V5.4 is installed already.
  3. Free update on DVD for a previously shipped STEP 7 V5.4 version via Internet order (customs and postage charges may become applicable for destinations outside the EU). To prove your procurement authorization for this free update you need to specify the license no. of your original software shipment of STEP 7 V5.4.
    Order_STEP7 ( 18 KB )
    You can also order an update on DVD for STEP 7 Professional 2006. To prove your procurement authorization for this free update you need to specify the license no. of your original software shipment of  STEP 7 Professional 2006.
    Order_STEP7_Professional ( 18 KB )  
     
    This method is recommended if you have updated your operating system from MS Windows XP to MS Windows Vista and STEP 7 or STEP 7 Professional are not yet installed on your PC.

 

Security information
In order to protect plants, systems, machines and networks against cyber threats, it is necessary to implement – and continuously maintain – a holistic, state-of-the-art industrial security concept. Siemens’ products and solutions constitute one element of such a concept. For more information about industrial security, please visit
http://www.siemens.com/industrialsecurity.