×
Siemens Industry Online Support
Siemens AG
Entry type: Product note Entry ID: 29830651, Entry date: 07/08/2008
(0)
Rate

Modifications Required when Using Type Rack 547B Basic Units for SIMATIC PCS 7 V6.0 + SP3

  • Entry
  • Associated product(s)

If you wish to expand installations employing SIMATIC PCS 7 V6.0 + SP3, you can use Type Rack 547B Basic Units based on Windows 2000 with pre-installed SIMATIC PCS 7 V6.1 + SP2 ES/OS software. However, these units must first be modified as described below.

The following Type Rack 547B basic units are available as replacements for the discontinued Type IL 43 basic units:
 

Discontinued Basic Units

Available Replacement Types

Designation

Order No.

Designation

Order No.

SIMATIC PCS 7 ES/OS IL 43 BCE W2K

6ES7 650-0LC16-0YX0 

deleted version

SIMATIC PCS 7 ES/OS IL 43 IE W2K

6ES7 650-0LC16-0YX1

SIMATIC PCS 7 ES/OS Rack 547B IE W2k

6ES7650-0NC16-0YX1

SIMATIC PCS 7 OS Client IL 43 W2K

6ES7 650-0LD16-0YX0

SIMATIC PCS 7 OS Client Rack 547B W2k

6ES7650-0ND16-0YX0

SIMATIC PCS 7 OS Server IL 43 BCE W2K

6ES7 650-0LE16-0YX0

deleted version

SIMATIC PCS 7 OS Server IL 43 IE W2K

6ES7 650-0LE16-0YX1

SIMATIC PCS 7 OS Server Rack 547B IE W2k

6ES7650-0NE16-0YX1

Due to the fact that the replacement types are equipped with the latest SIMATIC PCS 7 V6.1 + SP2 ES/OS software and the "IE" versions with a CP 1613 A2 communication module, they must be modified before use in installations with SIMATIC PCS 7 V6.0 + SP3.

The restore DVD A1 included in the scope of supply easily enables you to replace the existing ES/OS software installation by a pure Windows 2000 Professional / 2000 Server operating system and then install SIMATIC PCS 7 V6.0 + SP3 (incl. SQL Server, MS Patches, Post Fixes, etc).

Please proceed as follows:

1)

Load restore DVD A1

2)

Install SIMATIC PCS 7 V6.0 + SP3 in the usual sequence (SQL Server, MS Patches, PCS 7 V6.0 + SP3, Post Fixes – if necessary)

3)

Installation of CP 1613 A2:

 

The CP 1613 A2 communication module must be post installed with SIMATIC PCS 7 V6.0 + SP3. Two options exist:

 

a)

Installation via the PNP Wizard

 

 

1.

Message: "New hardware found"

 

 

2.

When the message "Ethernet Controller" comes up press "Next" button and then continue from 4. onwards (see below)

 

b)

Installation via the device manager

 

 

1.

Open the device manager: yellow exclamation mark displayed at "Other devices"

 

 

2.

Double click on "Ethernet Controller"

 

 

3.

Select the "Driver" tag in the "Features" dialog and click "Updating"

 

From now on the two dialogs are identical. Please proceed as follows:

 

 

4.

Select "Install software from a list or a particular source"

 

 

5.

Upon "also search in the following source" select the path "C:\Drivers\Network\Siemens\CP1613"
The driver for the CP1613 A2 is already located in the directory "C:\Drivers\Network\Siemens\CP1613"

 

 

6.

Select CP 1613 and continue with "OK"

 

 

7.

After completion of the installation: execute "Reboot"

Security information
In order to protect technical infrastructures, systems, machines and networks against cyber threats, it is necessary to implement – and continuously maintain – a holistic, state-of-the-art IT security concept. Siemens’ products and solutions constitute one element of such a concept. For more information about cyber security, please visit
https://www.siemens.com/cybersecurity#Ouraspiration.
Rate entry
no rating
Requests and feedback
What do you want to do?
Note: The feedback always relates to the current entry / product. Your message will be forwarded to our technical editors working in the Online Support. In a few days, you will receive a response if your feedback requires one. If we have no further questions, you will not hear from us.