×
Siemens Industry Online Support
Siemens AG
Тип сообщения: Часто задаваемые вопросы ID сообщения: 299124, Дата сообщения: 08.11.2010
(0)
Оценить

What is the maximum number of OPs that a CPU S7-300 can communicate with?

  • Сообщение
  • Относится к продукту(ам)

Description
The maximum number of OPs that a CPU S7-300 can communicate with depends on the connection resources of the CPU concerned in each case. Of the total number of connections there is a default setting always reserving one connection for the PC communication and one for the OP communication. No smaller value can be set. 

You can use the remaining connections for OP communication if you do not need any PG or S7 basic communication connections or are not implementing any CPs that might also occupy "Other Connection" (e.g. CP343-1 for communication with SEND/RECEIVE data lengths >240 bytes).

In many SIMATIC S7-300 CPUs (see table below) you can reserve connection resources for PG, OP, S7 Basic communication and routing.
 

CPU

Order number Number of connections

312

6ES7312-1AD10-0AB0
6ES7312-1AE1x-0AB0
6

312 C

6ES7312-5BD0x-0AB0
6ES7312-5BE03-0AB0
6

313 C

6ES7313-5BE0x-0AB0
6ES7313-5BF03-0AB0
8

313 C-2DP

6ES7313-6CE0x-0AB0
6ES7313-6CF03-0AB0
8

313 C-2PtP

6ES7313-6BE0x-0AB0
6ES7313-6BF03-0AB0
8

314

6ES7314-1AF1x-0AB0
6ES7314-1AG1x-0AB0
12

314 C-2DP

6ES7314-6CF0x-0AB0
6ES7314-6CG03-0AB0
12

314 C-2PtP

6ES7314-6BF0x-0AB0
6ES7314-6BG03-0AB0
12

315-2DP

6ES7315-2AG10-0AB0
6ES7315-2AH14-0AB0
16

315-2PN/DP

6ES7315-2EG10-0AB0
6ES7315-2EH1x-0AB0
16

315 F-2DP

6ES7315-6FF0x-0AB0 16

315 F-2PN/DP

6ES7315-2FH1x-0AB0
6ES7315-2FJ14-0AB0
16

315 T

6ES7315-6TG10-0AB0
6ES7315-6TH13-0AB0
16

317-2DP

6ES7317-2AJ10-0AB0 32

317-2PN/DP

6ES7317-2EJ10-0AB0
6ES7317-2EK1x-0AB0
32

317 F-2DP

6ES7317-6FF0x-0AB0 32

317 T

6ES7317-6TJ10-0AB0
6ES7317-6TK13-0AB0
32

317 F-2PN/DP

6ES7317-2FJ10-0AB0
6ES7317-2FK1x-0AB0
32

319-3PN/DP

6ES7318-3EL0x-0AB0 32

You can set the connections in the SIMATIC Manager via "HW Config > CPU > Properties > Communication".


Fig. 1: Settings of the connection resources

More information is available by pressing the Help button in the mask above and in the index of the STEP 7 Online Help under "Information on using connection resources".

If you have not reserved the maximum number of connections, it is possible to use all the connections that are still available to make use of the maximum number of connection resources. 

The example in the following figure shows that with the settings made there it is possible to set up a minimum of 4 and maximum of 6 connections to OPs.


Fig. 2: Setting options of the connection resources

The communication services occupy the connection resources in chronological order of the logons. If you attempt to set up more connections than there are resources available, these communication connections are only set up once existing connections have been cleared down and resources are made available again.
Depending on requirements in terms of response times, there are ways of increasing the number of connections:

  • Use a CPU with greater resources.
  • Use one or more CP 342-5s.
    It makes sense to connect several OPs to a CP because each CP occupies a connection.

S7 connections with PUT/GET functions do not occupy any connection resources, even if you have set up the connections earlier.

Note

  • More information on the connection resources of the CPU you are using is available in the device manual "S7-300, CPU 31xC and CPU 31x: Technical Data" in Entry ID:12996906.
  • General information on communication with SIMATIC is available in the manual "Communication with SIMATIC" (Entry D 1254686).

Указания по безопасности
Для обеспечения и дальнейшего поддержания кибер-безопасности технической инфраструктуры, систем, машин и сетей необходимо внедрить комплексную концепцию информационной безопасности, которая соответствует последним достижениям науки и техники. Продукты и решения Сименс являются всего лишь одним из компонентов такой концепции. Более подробную информацию о кибер-безопасности можно получить здесь
https://www.siemens.com/cybersecurity#Ouraspiration.
Оценить сообщение
без оценки
Вопросы и обратная связь
Что вы хотите сделать?
Примечание: отзыв всегда относится к текущей статье. Ваше сообщение будет отправлено редакторам службы онлайн-поддержки. В течение нескольких дней вы получите ответ, если ваш отзыв содержит вопрос. Если у нас не возникнут вопросы по вашему отзыву, мы не будем вас беспокоить.
Поддержка статистики
Данная функция позволяет выдавать идентификаторы (ID) результата поиска согласно желаемому количеству (формат .txt)

Генерировать список
Копировать URL
Отобразить эту страницу в новом дизайне
Панель управления mySupport
Тематические страницы для данных записей