×
Siemens Industry Online Support
Siemens AG
Entry type: FAQ Entry ID: 30319971, Entry date: 08/12/2008
(0)
Rate

Interdependence of size, output and torque

  • Entry
  • Associated product(s)

QUESTION:

 

 

 

 

 

What is the relationship between size, output and torque?


ANSWER / REMEDY / NOTES:

     

  

 

The spatial dimensions of an electrical machine are primarily determined by the torque.

Machines with the same torque have approximately the same dimensions.

 

 

The output of a machine is calculated as follows:

 

 

 

 

 

P

M

n

 in [kW]

 in [Nm]

 in [1/min]

     

 

 

It follows from this that machines with the same output have different torques at different speeds and therefore different dimensions as well.

Motors with high speeds have smaller dimensions and are therefore lighter than motors of the same output with low speeds.

     
   
     
   

Influence of torque on the motor size

     

Security information
In order to protect technical infrastructures, systems, machines and networks against cyber threats, it is necessary to implement – and continuously maintain – a holistic, state-of-the-art IT security concept. Siemens’ products and solutions constitute one element of such a concept. For more information about cyber security, please visit
https://www.siemens.com/cybersecurity#Ouraspiration.