×
Siemens Industry Online Support
Siemens AG
Entry type: FAQ Entry ID: 30320280, Entry date: 08/12/2008
(5)
Rate

What is an IM code, and what types of electrical machines are there?

  • Entry
  • Associated product(s)

QUESTION:

 

 

 

 

 

What is an IM code, and what types of electrical machines are there?


ANSWER / REMEDY / NOTES:

  

 

 

  

 

Type of construction and installation are identified with an inter-nationally standardized IM code in accordance with IEC 600 34-7.

 

 

 

This code takes into account:

  • The position of the motor shaft

  • The type of bearing shield

  • Fastening of the machine

  • Method of installation

  • Nature of the shaft end

 

 

 

The following characteristics are not recorded in the IM code and have to be agreed on:

  • Position of terminal box

  • Type of bearing

  • Shape of the shaft end

  • Position of the ventilation holes

  • Type of torque transmission, among other things

 

 

 

Code I:

Suitable for machines with bearing shields and one shaft end
           Code example: IM B3

 

 

 

     
 

 

Code II:

Suitable for all machines            Code example: IM 1001

 

   

 

 

 

 

 

Code I is preferred for describing the types of construction.

Code II is used in cases in which Code I is not sufficient for complete description of the type of construction.

     

 

Types of construction of motors are defined in the standard

IEC 600 34-7.

The most common types of construction at SIEMENS are:

 

(Statement of IEC 600 34-7)

 

Security information
In order to protect technical infrastructures, systems, machines and networks against cyber threats, it is necessary to implement – and continuously maintain – a holistic, state-of-the-art IT security concept. Siemens’ products and solutions constitute one element of such a concept. For more information about cyber security, please visit
https://www.siemens.com/cybersecurity#Ouraspiration.
Rate entry
no rating
Requests and feedback
What do you want to do?
Note: The feedback always relates to the current entry / product. Your message will be forwarded to our technical editors working in the Online Support. In a few days, you will receive a response if your feedback requires one. If we have no further questions, you will not hear from us.