×
Siemens Industry Online Support
Siemens AG
Entry type: Product note Entry ID: 30610962, Entry date: 10/13/2008
(0)
Rate

S7-PDIAG V5.3 SP3 Released for Delivery

  • Entry
  • Associated product(s)


S7-PDIAG is now available in the new version 5.3 SP3.


S7-PDIAG V5.3 SP3 has been released for the following operating systems:

MS Windows XP Professional, MS Windows Server 2003 (as workstation computer), MS Windows Vista 32-Bit Ultimate and Business

Customers with a valid Software Update Service agreement for S7-PDIAG will receive the update to S7-PDIAG V5.3SP3 automatically.


 
Delivery release for S7-PDIAG V5.3 SP3

Contents:

1. Ordering information on S7-PDIAG V5.3 SP3
2. New features compared to the predecessor version
3. System prerequisites
4. S7-PDIAG Product description
4.1 Summary of process diagnosis in plant
4.2 Configuration of S7-PDIAG process diagnosis
4.3 Interaction with SIMATIC HMI
4.4 SIMATIC S7-GRAPH and S7-HiGraph
5. Information on ProAgent


1. Ordering information on S7-PDIAG V5.3

Order No.

Designation

6ES7840-0CC04-0YA5

SIMATIC S7, S7-PDIAG V5.3 incl. SP3
FLOATING LICENSE FOR 1 USER

6ES7840-0CC04-0YE5

SIMATIC S7, S7-PDIAG V5.3 incl. SP3 UPGRADE
(V3.X - V5.1 to V5.3 SP3)
FLOATING LICENSE FOR 1 USER

6ES7840-0CC04-2YN8

SIMATIC S7, S7-PDIAG V5.3 
UNLOCK COPY LICENSE, ONLY VALID IN CONJUNCTION WITH UNLOCK COPY LICENSE AGREEMENT AND VALID LICENSE

6ES7840-0CA01-0YX2

SIMATIC S7, S7-PDIAG SOFTWARE UPDATE SERVICE FOR 1 YEAR WITH AUTOM. EXTENSION, CURRENT SW VERSION IS MANDATORY


S7-PDIAG V5.3 SP3 Upgrade:

Customers who use S7-PDIAG V3.x, V4.x, V5.0 or V5.1 already, can purchase an upgrade. The precondition for installation of the upgrade package is a valid license for S7-PDIAG V3.x, V4.x, V5.0, V5.1 or V5.3.  

General:

S7-PDIAG V5.3 SP3 is supplied on a CD, the license key (Automation License Key) is supplied on a USB stick. S7-PDIAG V5.3 SP3 is multilingual (G, E, F, I, Sp). 

Documentation:

The documentation for S7-PDIAG V5.3 SP3 is supplied as PDF file on the product CD. It is not available in printed form. 

2. New features compared to the predecessor version

New in S7-PDIAG V5.3 SP3

  • Enhanced search function
    The search for S7-PDIAG error definitions with possibly uncomplete configuration has been enhanced for the following points:
    • For error definitions which have not selected initial value recording.
    • For error definitions defined in a global DB.
    • For error definitions defined directly under the standard group.

In these cases the complete S7 program will be scrutinized.

 

New in S7-PDIAG V5.3 SP2

 

New in S7-PDIAG V5.3 SP1

  • Monitoring and acknowledgement status
    • S7-PDIAG Error definitions were augmented by the attributes "Monitoring status" and "Acknowledgement status". Operands can be allocated to these attributes in the monitoring configuration. The status of monitoring and the status of acknowledgement are thus available in the user program. The operands are entered in the reference data.
  • Extension of the dialog field "Search in - ..." and the associated processing dialogs
    • The message attributes "Message class", "Acknowledgement group" and "Logging", as well as the monitoring and acknowledgement status were newly added to the dialog "Search in -..." and the associated processing dialogs.
    • Search for S7-PDIAG error definitions with possibly incomplete configuration. These error definitions can be displayed, processed and deleted in the dialog field "Search in -...", together with the possible cause.
    • The columns displayed in the dialog field "Search in -..." can be faded in or out via the context menu.

Since S7-PDIAG V5.3

  • Changeover for S7-PDIAG to the new license types Floating License and Trial License. Licensing with the Automation License Manager.
  • Inconsistency warning when loading modified blocks. The offline blocks in STEP7 are considered
    (no automatic online / offline comparison).
  • Support of  foreign-language character sets as introduced with STEP7 V5.3 SP2.
  • Changeover of S7-PDIAG to the STL compiler
    Avoids previous restrictions when allocating names for FB variables
    Reduces the block size of the monitoring blocks
    Expands the permitted data types of the collateral values by CHAR, INT, DINT and REAL.

 

3. System prerequisites

Supported operating systems

  • MS Windows XP Professional
  • MS Windows Server 2003 (as workstation)
  • MS Windows Vista 32-bit Ultimate and Business

STEP 7:

  • STEP 7 V5.3 SP3 and higher

4. S7-PDIAG Product description

4.1 Summary of process diagnostics in plant operation

The purpose of process diagnostics is to evaluate process faults outside the automation system. Examples are

  • Limit switch not reached
  • Interlock not fulfilled
  • Watchdog time elapsed
  • Motion interrupted
From that follows:
  • Identify fault – save process signals when the fault occurs
  • Signal fault – message to SIMATIC HMI system and display cause of the fault (criteria analysis)
  • Remove fault – by operating certain equipment in manual mode
  • Continue with the process – resume production after a short standstill

4.2 Configuration of S7-PDIAG process diagnosis

S7-PDIAG provides powerful configuration options in LAD, FBD and STL programming languages for this purpose. When generating the program, the user can configure various types of monitoring for critical process signals in STEP 7. Generation of the associated monitoring logic and actual value detection (by function blocks) is done automatically by S7-PDIAG. In addition, S7-PDIAG enables the control of movements in manual operating mode via UDT interface (User Defined Type). A movement can thus be controlled directly from the SIMATIC HMI system. Similarly, an operating mode interface permits switching over directly on the SIMATIC HMI.

4.3 Interaction with SIMATIC HMI

The software package SIMATIC ProAgent for OP/TP/MP/PC and WinCC rounds off process diagnosis with the following functions:

  • Display of process faults (configured with S7-PDIAG)
  • Determination of the cause of the fault
  • Operating mode changeover
  • Support with fault correction (control of manual movements)
SIMATIC Process diagnostics presupposes a uniform siganalling path (Alarm_S/SQ, or D/DQ: operating system function of the S7-CPU). This event-controlled siganalling path is a basic means to enable selective and fast diagnosis in plants and machines.
S7-PDIAG and ProAgent thus:

  • efficiently support troubleshooting and fault correction
  • increase the availability of plant and machines
  • help to reduce downtimes

4.4 SIMATIC S7-GRAPH and S7-HiGraph

SIMATIC Process diagnosis also includes the engineering tools S7-GRAPH and S7-HiGraph. S7-PDIAG is not required if the process diagnostics functions with S7-GRAPH or S7-HiGraph and ProAgent are used. 5. Information on ProAgent

The ProAgent optional software package was specially tailored for S7-PDIAG, S7-GRAPH and S7-HiGraph (only ProAgent/MP and ProAgent/PC) and supplements process diagnosis with the following features:

  • ProAgent can be loaded with the configuration software ProTool, ProTool/Pro, WinCCflexible or WinCC
  • Can be used for graphic HMI panels (as from 270/277 range) and WinCC  
  • Easy acces to process diagnostic data
  • Uniform technological view on process diagnostics
  • The following standard screenforms are available:
    • easy to use message screen with softkeys and filter functions
    • overview screen with technological view on the process
    • detailed diagnostic screen for selective determination of the cause of the fault
    • motion screen for fault correction support.
    • operation of certain equipment in manual mode.

Please get in touch with your SIMATIC contact at your local Siemens Office if you have any further questions.

Siemens partners on the Internet


Security information
In order to protect technical infrastructures, systems, machines and networks against cyber threats, it is necessary to implement – and continuously maintain – a holistic, state-of-the-art IT security concept. Siemens’ products and solutions constitute one element of such a concept. For more information about cyber security, please visit
https://www.siemens.com/cybersecurity#Ouraspiration.