×
Siemens Industry Online Support
Siemens AG
Entry type: FAQ Entry ID: 31092306, Entry date: 09/18/2008
(0)
Rate

Procedure with belt pulleys

  • Entry
  • Associated product(s)

 

QUESTION:

 

 

 

 

 

What do I need to be aware of with belt pulleys?


ANSWER / REMEDY / NOTES:

     
   

 

 

 

 

 

V-belt pulley and forces acting on V-belt

 

 

 

 

 

For a given motor, belt pulleys with the smallest possible diameter are the ideal, as these allow the driven pulley to be kept as small as possible. However, these result in increased transverse force on the motor shaft.

Belt pulleys should therefore always be slid up against the shaft shoulder of the motor in order to keep the bending fatigue load of the shaft as low as possible.

Only those kinds of belt pulleys on which the line of action of the transverse force lies within the free motor shaft extension may be used.

 

 

 

Security information
In order to protect technical infrastructures, systems, machines and networks against cyber threats, it is necessary to implement – and continuously maintain – a holistic, state-of-the-art IT security concept. Siemens’ products and solutions constitute one element of such a concept. For more information about cyber security, please visit