×
Siemens Industry Online Support
Siemens AG
Entry type: Application example Entry ID: 31410726, Entry date: 02/16/2012
(2)
Rate

Safety Integrated in combination with SIMOTION D435; activation of safety functions with TM54F

  • Entry
  • Associated product(s)

Task:
A system equipped with SINAMICS S120 drives is controlled by a SIMOTION D435. This system requires various system functions.

The SIMOTION does not provide integrated safety functions. It uses the extended safety functions integrated in the SINAMICS S120 drives.

These safety functions are activated via the failsafe Terminal Module TM54F. Failsafe signals are preprocessed in a SIMATIC F-CPU.

Solution:
This functional example describes in detail how to configure the failsafe SIMATIC CPU, the safety functions integrated in the drives and the TM54F as well as the handling by SIMOTION.

This functional example is based on the SIMOTION training case and the Safety training case. The configuration must be adapted when using other hardware.

See the following documentation:

Downloads

Content of the Downloads

Download

Documentation 31410726_mc_fe_i_007_v12_en.pdf ( 6933 KB )
Project MC_FE_I_007_V10_EN.zip ( 1569 KB )

Last Changes
V1.2, revised documentation

Search term
motioncontrol_apc_applications

 

Security information
In order to protect technical infrastructures, systems, machines and networks against cyber threats, it is necessary to implement – and continuously maintain – a holistic, state-of-the-art IT security concept. Siemens’ products and solutions constitute one element of such a concept. For more information about cyber security, please visit
https://www.siemens.com/cybersecurity#Ouraspiration.
Rate entry
no rating
Requests and feedback
What do you want to do?
Note: The feedback always relates to the current entry / product. Your message will be forwarded to our technical editors working in the Online Support. In a few days, you will receive a response if your feedback requires one. If we have no further questions, you will not hear from us.