Entry type: Download, Entry ID: 109311724, Entry date: 07/20/2015
(49)
Rate

Updates for STEP 7 V13 SP1 and WinCC V13 SP1

  • Entry
  • Associated product(s)
Status July 2015: Update 4

This update is valid for the following products in the TIA Portal

  • STEP 7 Basic/Professional V13 SP1
  • WinCC Basic/Comfort/Advanced/Professional V13 SP1

 

Installation instructions:

  • Updates are cumulative and contains all previous updates

  • The update can only be installed if one of the products mentioned above is already installed.

  • After each installation of STEP 7 V13 SP1 or WinCC V13 SP1, the latest update needs to be installed. 

 

You can find updates for TIA Portal Openness in the following entry 109477177

You can find updates for STEP 7 Safety V13 SP1 in the following entry 109477092

You can find updates for WinCC Runtime Professional V13 SP1 in the following entry 109439573

You can find updates for WinCC Runtime Advanced V13 SP1 in the following entry 109311423

 

_______________________________________________________________________________

Update 4 (07/2015)

Improvements compared to earlier versions:

  see readme file of Update 4 (166,1 KB)

 

Installation instructions:

  • The download is divided into several files. Please download all the files into the same directory and execute the file ending with .exe. The files will now be combined and you can execute the setup.

  • If you are using and have installed STEP 7 Safety, please note that, in addition to the TIA Portal Update 4, installation of STEP 7 Safety Update 4 is also essential. If the versions do not match, this would prevent the TIA Portal from starting.


Update 4 for STEP 7 V13 SP1 / WinCC V13 SP1 (07/2015):

  Totally_Integrated_Automation_Portal_V13_SP1_Upd4.001 (1,8 GB)

  Totally_Integrated_Automation_Portal_V13_SP1_Upd4.002 (230,2 MB)

  Totally_Integrated_Automation_Portal_V13_SP1_Upd4.exe (2,6 MB)

 

_______________________________________________________________________________

Update 3 (05/2015)

Improvements compared to earlier versions:

see readme file of Update 3 (226.8 KB)

Update 3 for STEP 7 V13 SP1 / WinCC V13 SP1:

Totally_Integrated_Automation_Portal_V13_SP1_Upd3.exe, (1.3 GB)

 

_______________________________________________________________________________

Update 2 (04/2015)

Improvements compared to earlier versions:

see readme file of Update 2 (130.3 KB).


Update 2 for STEP 7 V13 SP1 / WinCC V13 SP1:

Totally_Integrated_Automation_Portal_V13_SP1_Upd2.exe (959.5 MB)

 

_______________________________________________________________________________

Update 1

Improvements compared to earlier versions:

  see readme file of Update 1 (179,9 KB)


Update 1 for STEP 7 V13 SP1 / WinCC V13 SP1 :

 Totally_Integrated_Automation_Portal_V13_SP1_Upd1.exe (542.5 MB)

 

_______________________________________________________________________________