×
Siemens Industry Online Support
Siemens AG
Entry type: Download Entry ID: 31622426, Entry date: 10/09/2014
(9)
Rate

EPLAN Electric P8 macros for SIMOTION C, P and D / DXF files

  • Entry
  • Associated product(s)

EPLAN Electric P8 is an CAE system to engineer electrical plants and systems (e.g. control cabinets). It supports the design engineer when engineering, documenting and managing projects. Using EPLAN Electric P8, customers create circuit diagrams of the control cabinet, manage the parts master data, automatically generate parts lists, terminal diagrams, PLC diagrams and overview diagrams, generate documentation for the plant/system and carry out the mechanical design of the control cabinet.

Especially more complex devices (e.g. controllers and frequency converters) are not available in EPLAN as standard symbol. As a consequence, users must create these themselves as macros. Macros allow users to define frequently used modules (parts of circuits, graphic elements, etc.) of their projects as macro. These are then saved and can be reused as often as required.

Providing EPLAN Electric P8 macros in the .edz format helps customers significantly reduce their engineering time.

In order to keep the costs associated with integrating data into the EPLAN system as low as possible, it must be simple and quick to import data.
For this reason Siemens requested that EPLAN introduce a new file format (.edz file), which provides a file with all of the required information for every order number. This means that an .edz file is a type of archive for master parts data, macros and other CAx data. A macro in the edz format contains the following data:

 

EPLAN Electric P8 macros in the new .edz format

EPLAN Electric P8 macros in the new .edz format can be odered at the following Internet addresses:

 

EPLAN Electric P8 macros in the existing .ema format
The existing macros in the .ema format are still available for download. Please note that these macros will no longer be updated.

SIMOTION_EPLANP8_MAKROS_V004.pdf ( 4099 KB )

SIMOTION_EPLANP8_MAKROS_V004.zip ( 10419 KB )

DXF_Files_V004.zip ( 2698 KB )

 

NOTE

The information contained in this documentation refers to standard configurations and comprises general descriptions or performance characteristics which may not always be applicable in the described form to the specific application case or which may change due to product advancement. The performance characteristics are exemplary for selected products or application cases or describe technical possibilities. As for the rest, the General Terms of Use apply accordingly.

Security information
In order to protect technical infrastructures, systems, machines and networks against cyber threats, it is necessary to implement – and continuously maintain – a holistic, state-of-the-art IT security concept. Siemens’ products and solutions constitute one element of such a concept. For more information about cyber security, please visit
https://www.siemens.com/cybersecurity#Ouraspiration.