×
Siemens Industry Online Support
Siemens AG
Entry type: Application example Entry ID: 31624179, Entry date: 10/27/2015
(31)
Rate

Example blocks for WinCC V7 and STEP 7 V13 (TIA Portal) for S7-1200 and S7-1500 in SCL

  • Entry
  • Associated product(s)
This documentation shows how WinCC V7.3 SE and TIA Portal STEP 7 Professional V13 SP1 with example blocks is used for the solution of an technological automation task.

The sensors and actuators of a plant system represent the basis of the most automation projects. In the standard delivery of STEP 7 Professional V13 SP1 and WinCC V7.3 SE, there are no technological blocks contained.
At this point, this application example provides a remedy. It makes useful blocks available for
WinCC V7.3 SE and STEP 7 Professional V13 SP1 with S7-1500 systems.

Solution
The documentation describes how the technological blocks are called and interconnected in STEP 7 Professional V13 SP1 and WinCC V7.3 SE.
This example project also shows the ready interconnection of the technology blocks (basic automation).

  • VALVE
    Visualization and operation of a binary valve
  • DIGITALL
    Visualization and operation of digital signals.
  • ANALOGUE
    Visualization and operation of analog signals.
  • MOTOR
    Visualization and operation of a motor with fixed speed and rotational direction.

To do so, an example plant has been configured which includes several binary and analog values, valves and motors. This example project also shows how the individual technology blocks are interconnected (basic automation). Higher-level automation functions (two-step and PID control) are also configured.

The figure below shows exemplary faceplates of the solutions.

Downloads
 Registrierung notwendig Documentation (5,0 MB)
 Registrierung notwendig  Templates for WinCC V7.3 SE (1,1 MB)
 Registrierung notwendig PLC blocks STEP 7 V13 SP1 (1,3 MB)
 Registrierung notwendig  Sample project (43,2 MB)
The sample project shows the use of the blocks.

  • Demoproject WinCC V7.3 SE
  • Demoproject STEP 7 TIA Portal V 13 SP1

Further Example Blocks

Further Informationen


Last Changes
Update to WinCC V7.3 SE and STEP 7 V13 SP1.

Additional Keywords
Faceplate, creating faceplates, FPT, sample project, screen block, sample program

 

Security information
In order to protect technical infrastructures, systems, machines and networks against cyber threats, it is necessary to implement – and continuously maintain – a holistic, state-of-the-art IT security concept. Siemens’ products and solutions constitute one element of such a concept. For more information about cyber security, please visit
http://www.siemens.com/industrialsecurity.