×
Siemens Industry Online Support
Siemens AG
文档类型 常问问题 文档编号 31644110, 文档发布日期 2008年9月25日
(0)
评估

Relation between selecting a machine bearing and its coupling versions

  • 文档
  • 涉及产品

 

QUESTION:

 

 

 

 

 

What relation is there between selecting a machine bearing and its coupling versions?


ANSWER / REMEDY / NOTES:

     

  

 

Motors with rolling-contact bearings always use an axial guide bearing (location bearing) and always require an axially flexible coupling due to the thermal expansion of the shafts.

 

 

 

 

 

Motors with sliding bearings are designed with two floating bearings as standard. The rotor is guided axially by the axial guide bearing of the machine or the gearbox. An axially limiting coupling is required so that the bearing shell in the motor bearing on the DE side does not axially run against the shaft shoulder.

The dimensions of the axial limitation are specified in the machine manual.

 

 

Motors with sliding bearings and axial guide bearing (special design) must have an highly axially flexible and highly elastic coupling due to the thermal expansion of the shafts.

 

 

 

   

Motors with cylindrical-roller bearing and coupling output

Couplings cause low radial loads.

Cylindrical-roller bearings on the other hand require a certain minimum load for a smooth rolling. If this minimum load is not applied, the bearings become noisy (screech) and wear prematurely.

Deep-groove ball bearings are therefore the preferred type of rolling-contact bearing for coupling outputs.

The use of motors with cylindrical-roller bearings on coupling outputs should always be clarified with the motor manufacturer.

 

 

 

   

Motors with cylindrical-roller bearing and coupling output

Couplings cause low radial loads.

Cylindrical-roller bearings on the other hand require a certain minimum load for a smooth rolling. If this minimum load is not applied, the bearings become noisy (screech) and wear prematurely.

Deep-groove ball bearings are therefore the preferred type of rolling-contact bearing for coupling outputs.

The use of motors with cylindrical-roller bearings on coupling outputs should always be clarified with the motor manufacturer.

 

 

 

安全性信息
为了保护技术基础设施、系统、机器和网络免受网络威胁,有必要实施并持续维护一个全面、最先进的IT安全方案。西门子的产品和解决方案构成了这一方案的一个要素。有关网络安全的更多信息,请访问
https://www.siemens.com/cybersecurity#Ouraspiration.
对统计的支持
用该功能可根据所需数量输出搜索结果的IDs (格式 .txt)

生成列表
复制URL
在新设计中显示此页面
mySupport Cockpit
相关链接