×
Siemens Industry Online Support
Siemens AG
Entry type: Download Entry ID: 31674577, Entry date: 02/26/2021
(8)
Rate

Firmware Update PAC3200 Power Monitoring

  • Entry
  • Associated product(s)
Firmware Update PAC3200 Power Monitoring

Description:

If the device firmware is updated, the respective firmware always has to be updated to the latest version available for the PAC3200.

Please note that a firmware update may also require a new version of the language package.

The update can be performed by application of the configuration software SENTRON powerconfig, which is included in the scope of supply or available in the Internet. A description of the update procedure can be found in the online help of the software.

Newest version:



Update V2.4.7
 (7KM2111-1BA00-3AA0, 7KM2112-0BA00-2AA0, 7KM2112-0BA00-3AA0)

The firmware update V2.4.7 incorporates the following modification: Small optimizations

Note!

  • After updating the PAC 3200 to firmware V2.4.7 it is not necessary to update a new language package
  • After updating to the firmware version V2.4.7 an older version (<V2.4.7) must not be loaded because this would lead to an irreversible malfunction of the device
  • The use of the latest Powerconfig version is recommended


DOWNLOAD:

Applikationsfirmware Version: V2.4.7 (02/2021)
7KM2111-1BA00-3AA0, 7KM2112-0BA00-2AA0, 7KM2112-0BA00-3AA0

 Registrierung notwendig  PAC3200fw_V2.4.7.zip (101,1 KB)


SHA-256 checksum:

 Registrierung notwendig  PAC3200fw_V2.4.7-0.0.3.0.bin.txt (1 KB)
Information about SHA-256


Readme Open Source Software (OSS)

 Registrierung notwendig  7KM_PAC3200_Readme_OSS.zip (152,7 KB

Older version:

Update V2.4.6
 (7KM2111-1BA00-3AA0, 7KM2112-0BA00-2AA0, 7KM2112-0BA00-3AA0)

The firmware update V2.4.6 incorporates the following modification:

  • Support ethernet link up for switches with configured vlan
  • Fix polish language pack in LP2

 
Note!

  • After updating the PAC 3200 to firmware V2.4.6 it is not necessary to update a new language package
  • Use the new LP2 language pac for polish language
  • The use of the latest Powerconfig version is recommended
Update V2.4.5
 (7KM2111-1BA00-3AA0, 7KM2112-0BA00-2AA0, 7KM2112-0BA00-3AA0)

The firmware update V2.4.5 incorporates the following modification:

  • Support for baudrates up to 115200 for module slot communication
  • Support for 3 simultaneous Modbus/TCP connections
  • Random initial sequence number for TCP

 
Note!

  • After updating the PAC 3200 to firmware V2.4.5 it is not necessary to update a new language package
  • The use of the latest Powerconfig version is recommended
Update V2.4.4
 (7KM2111-1BA00-3AA0, 7KM2112-0BA00-2AA0, 7KM2112-0BA00-3AA0)

The firmware update V2.4.4 incorporates the following modification: Small optimizations
 
Note!

  • After updating the PAC 3200 to firmware V2.4.4 it is imperative to update the language package to version V2.4.3! The related language package can also be found on this download page.
  • After updating to the firmware version V.2.4.4, an older version (<V2.4.4) must not be loaded because this would lead to an irreversible malfunction of the device.

Update V2.4.3
 (7KM2111-1BA00-3AA0, 7KM2112-0BA00-2AA0, 7KM2112-0BA00-3AA0)

The firmware update V2.4.3 incorporates the following modification: Small optimizations
 
Note!

  • After updating the PAC 3200 to firmware V2.4.3 it is imperative to update the language package to version V2.4.3! The related language package can also be found on this download page.
  • After updating to the firmware version V.2.4.3, an older version (<V2.4.3) must not be loaded because this would lead to an irreversible malfunction of the device.


Update V2.4.2
 (7KM2111-1BA00-3AA0, 7KM2112-0BA00-2AA0, 7KM2112-0BA00-3AA0)

The firmware update V2.4.2 incorporates the following modification: Small optimizations
 
Note!

  • After updating the PAC 3200 to firmware V2.4.2 it is not necessary to update a new language package.
  • The use of the latest Powerconfig version is recommended.


Update V2.4.1
 (7KM2111-1BA00-3AA0, 7KM2112-0BA00-2AA0, 7KM2112-0BA00-3AA0)

The firmware update V2.4.1 incorporates the following modification: Small optimizations
 
Note!

  • After updating the PAC 3200 to firmware V2.4.1 it is not necessary to update a new language package.
  • The use of the latest Powerconfig version is recommended.


Update V2.4.0
(7KM2111-1BA00-3AA0, 7KM2112-0BA00-2AA0, 7KM2112-0BA00-3AA0)

The firmware update V2.4.0 incorporates the following modification: Small optimizations
 
Note!

  • After updating the PAC 3200 to firmware V2.4.0 it is not necessary to update a new language package.
  • The use of the latest Powerconfig version is recommended.


Update V2.3.5
 (7KM2111-1BA00-3AA0, 7KM2112-0BA00-2AA0, 7KM2112-0BA00-3AA0)

The firmware update V2.3.5 incorporates the following modification:

  • Detection of ethernet cable link and reinitialization at change of link status added.
  • Ethernet performance optimizes


Note!

  • After updating the PAC 3200 to firmware V2.3.5 it is not necessary to update a new language package.


Update V2.3.3
 (7KM2111-1BA00-3AA0, 7KM2112-0BA00-2AA0, 7KM2112-0BA00-3AA0)

The firmware update V2.3.3 incorporates the following modification:

  • Detection of ethernet cable link and reinitialization at change of link status added.
  • Ethernet performance optimizes


Note!

  • After updating the PAC 3200 to firmware V2.3.2 it is not necessary to update a new language package.


Update V2.3.0
 (7KM2111-1BA00-3AA0, 7KM2112-0BA00-2AA0, 7KM2112-0BA00-3AA0)

The above-specified version does not include any functional innovations.

Firmware Version V2.3.0 is mandatory in combination with PAC extension module PROFIBUS DPV1 V4.0 (7KM9300-0AB01-0AA0) along with powerconfig ≥V3.1, in order to configurate via PROFIBUS DP and to display measurement values.


Further information:
/cs/document/88779638?caller=view&lc=de-WW



Update V2.2.2
 (7KM2111-1BA00-3AA0, 7KM2112-0BA00-2AA0, 7KM2112-0BA00-3AA0)

The above-specified version does not include any functional innovations.

Firmware update V2.2.2 incorporates the following modifications:

  • Module connection optimized
  • Reset I&M1-4 by "return to factory settings" (PNO requirement)
  • I&M0 = 0x001E (PNO requirement)

The PAC3200 FW V.2.2.2 is recommended in combination with Modbus RTU module.


Update V2.2.1
 (7KM2111-1BA00-3AA0, 7KM2112-0BA00-2AA0, 7KM2112-0BA00-3AA0)

The above-specified version does not include any functional innovations.

Firmware update V2.2.1 incorporates the following modifications:

  • Optimization of S7 OpenModbus/TCP

The PAC3200 FW V.2.2.1 is recommended for S7 OpenModbus/TCP modules.


Update V2.2.0
 (7KM2111-1BA00-3AA0, 7KM2112-0BA00-2AA0, 7KM2112-0BA00-3AA0)

The above-stated version contains the following functional innovations:

  • Full support of modul „Switched Ethernet PROFINET“ (7KM9300-0AE00-0AA0).
  • New parameter “system phase angle” with selection of settings 120° (default), 180° or AUTO.


Firmware update V2.2.0 incorporates the following modifications:

  • Extented display of decimal places at current and power measurement.
  • Default display considering the connection type.
  • Detailed descriptions are available in the customer documentations.


Note!

  1. After updating the PAC4200 to firmware V2.2.0 it is imperative to update the language package to version V2.2.0! The related language package can also be found on this download page.
  2. After updating to the firmware version V2.2.0, an older version (≤1.1.x) must not be loaded because this would lead to an irreversible malfunction of the device.

Update V2.1.0
 (7KM2111-1BA00-3AA0, 7KM2112-0BA00-2AA0, 7KM2112-0BA00-3AA0)

The above-stated version contains the following functional innovations:

  • The power monitoring devices are now also available as 32-bit values via Modbus TCP or Modbus RTU (in connection with the expansion module PAC RS485). With the help of the function codes 0x03 and 0x04, these data can be read out from the following tabs:
 OffsetNumber of tabs Name  Format Unit Value rangeAccess 
 2801 2 Active power import tariff 1 Float Wh

Overflow

1.0e+12 

 R
 2803 2 Active power import tariff 2 Float Wh Overflow

1.0e+12 

 R
 2805 2 Active power import tariff 1 Float Wh

Overflow

1.0e+12 

 R
 2807 2 Active power import tariff 2 Float Wh Overflow

1.0e+12 

 R
 2809 2 Active power import tariff 1 Float varh Overflow

1.0e+12 

 R
 2811 2 Active power import tariff 2 Float varh Overflow

1.0e+12 

 R
 2813 2 Active power import tariff 1 Float varh Overflow

1.0e+12 

 R
 2815 2 Active power import tariff 2 Float varh Overflow

1.0e+12 

 R
 2817 2 Active power import tariff 1 Float VAh Overflow

1.0e+12 

 R
 2819 2 Active power import tariff 2 Float VAh

Overflow

1.0e+12 

 R
  • Also see chapter “Modbus TCP“ in the SENTRON PAC3200 manual.


The following changes are introduced by the firmware update V2.1.0:

  • Display brightness changes via the interface are also immediately saved in the setting menu.
  • The Modbus command 0x06 (reset) no longer resets the communication parameters for Modbus RTU.
  • If the entry “DEFAULT SETTINGS” is selected in the device menu < RESET >, the Modbus communication parameter are not reset. This both applies to the Modbus TCP parameters on the integrated Ethernet interface as well as to the Modbus RTU parameters in connection with the expansion module PAC RS485.


! Requires installation of a language package version V1.1.x or higher !
 

Update V2.0.12
 (7KM2111-1BA00-3AA0, 7KM2112-0BA00-2AA0, 7KM2112-0BA00-3AA0)

The above-specified version does not include any functional innovations.


Firmware update V2.0.12 incorporates the following modifications:

  • The calculation error concerning the total power of circuit variants 3P3WB and 3P4WB (measuring on symmetric loads with only one current transformer) has been corrected. For the total system power, three times the value of the single-phase power is now displayed.
  • The faulty pulse output of working pulses at the digital output during energy recovery has been corrected.
  • The device password for protection against impermissible parameter changes at the device can be set between 0000 and 9999 via communication interfaces.


! Requires installation of a language package, version V1.1.x or higher !


Update V2.0.8
 (7KM2111-1BA00-3AA0, 7KM2112-0BA00-2AA0, 7KM2112-0BA00-3AA0)

The above-specified version does not include any functional innovations.


Firmware update V2.0.8 incorporates the following modifications:

  • The safety monitoring of the voltage inputs (signal: “overcharged voltage”) for devices with extra-low voltage power supply (22…65V DC) has been adjusted. The maximum secondary rated voltage for direct measuring cannot be set to a value higher than 500V via communication interfaces.


Update V2.0.6
 (7KM2111-1BA00-3AA0, 7KM2112-0BA00-2AA0, 7KM2112-0BA00-3AA0)

The above-specified version does not include any functional innovations.


Firmware update V2.0.6 incorporates the following modifications:

  • Stabilization of TCP communication if inactivity on the Ethernet interface takes longer than ~120 seconds
  • The selection box “current transformer measuring yes/no”in the menu “current input 23.1“ has been removed.


Update V2.0.4
 (7KM2111-1BA00-3AA0, 7KM2112-0BA00-2AA0, 7KM2112-0BA00-3AA0)

The above-specified version includes the following functional innovations:

  • Introduction of subsequently loadable language packages
  • Display texts available in additional languages: French, Spanish, Italian, Portuguese, Turkish, Russian, Chinese.
  • Extension of the Ethernet interface by Modbus TCP and SEAbus TCP protocols


Update V1.0.0
 (7KM2111-1BA00-3AA0, 7KM2112-0BA00-2AA0, 7KM2112-0BA00-3AA0)
  • Primary edition of the application software
  • Display texts in German or English
  • Ethernet interface with proprietary protocol for communication between PAC3200 and the configuration software SENTRON powerconfig


Update V1.0.0
(7KM2111-1BA00-3AA0, 7KM2112-0BA00-2AA0, 7KM2112-0BA00-3AA0)

Der obige Ausgabestand beinhaltet keine funktionalen Neuerungen:

  • Erstausgabe der Applikationssoftware.
  • Anzeigentexte in Deutsch oder Englisch.
  • Ethernetschnittstelle mit proprietärem Protokoll zur Kommunikation zwischen PAC3200 und der Konfigurationssoftware SENTRON powerconfig.



Update V1.0.0
(7KM2111-1BA00-3AA0, 7KM2112-0BA00-2AA0, 7KM2112-0BA00-3AA0)

Der obige Ausgabestand beinhaltet keine funktionalen Neuerungen:

  • Erstausgabe der Applikationssoftware.
  • Anzeigentexte in Deutsch oder Englisch.
  • Ethernetschnittstelle mit proprietärem Protokoll zur Kommunikation zwischen PAC3200 und der Konfigurationssoftware SENTRON powerconfig.



Update V1.0.0
(7KM2111-1BA00-3AA0, 7KM2112-0BA00-2AA0, 7KM2112-0BA00-3AA0)

Der obige Ausgabestand beinhaltet keine funktionalen Neuerungen:

  • Erstausgabe der Applikationssoftware.
  • Anzeigentexte in Deutsch oder Englisch.
  • Ethernetschnittstelle mit proprietärem Protokoll zur Kommunikation zwischen PAC3200 und der Konfigurationssoftware SENTRON powerconfig.




Security information
In order to protect technical infrastructures, systems, machines and networks against cyber threats, it is necessary to implement – and continuously maintain – a holistic, state-of-the-art IT security concept. Siemens’ products and solutions constitute one element of such a concept. For more information about cyber security, please visit
https://www.siemens.com/cybersecurity#Ouraspiration.
Rate entry
no rating
Requests and feedback
What do you want to do?
Note: The feedback always relates to the current entry / product. Your message will be forwarded to our technical editors working in the Online Support. In a few days, you will receive a response if your feedback requires one. If we have no further questions, you will not hear from us.