×
Siemens Industry Online Support
Siemens AG
Entry type: Download Entry ID: 31676289, Entry date: 05/05/2017
(2)
Rate

Language Packages for PAC3200 Power Montitoring Device

  • Entry
  • Associated product(s)
Language Packages for PAC3200 Power Montitoring Device

Description:

For SENTRON PAC3200, two different language packages are available. With these packages, text displays on the device can be set to German, English, French, Spanish, Italian, Portuguese, Turkish, Chinese, Russian and Polish.

 If language packages are updated, the respective package always has to be updated to the latest version available for the PAC3200. Depending on the language package, one of the two language packages can be loaded into the device by application of the configuration software SENTRON powerconfig, which is included in the scope of supply or available in the Internet. A description of the update procedure is available in the online help of the software.


Language Package #1: V2.4.3: DE / EN / FR / ES / IT / PT / TR / ZH
 (7KM2111-1BA00-3AA0, 7KM2112-0BA00-2AA0, 7KM2112-0BA00-3AA0)

The standard language package (as-delivered condition ex works) contains the following languages:
German, English, French, Spanish, Italian, Portuguese, Turkish, Chinese 


Description:

Language package (DE / EN / FR / ES / IT / PT / TR / ZH) Version: 2.4.3 (03/2017)
PAC3200, 7KM2111-1BA00-3AA0, 7KM2112-0BA00-2AA0, 7KM2112-0BA00-3AA0

 

 Registrierung notwendig  PAC3200lp1_V2_4_3.zip (14,2 KB)


Language Package #2: V2.4.3:DE / EN / FR / TR / RU / ZH / PL
 (7KM2111-1BA00-3AA0, 7KM2112-0BA00-2AA0, 7KM2112-0BA00-3AA0)

Language package 2 contains the following languages:
German, English, French, Turkish, Russian, Chinese, Polish


Description:

Language package (DE / EN / FR / TR / RU / ZH / PL)Version: 2.4.3 (03/2017)

PAC3200, 7KM2111-1BA00-3AA0, 7KM2112-0BA00-2AA0, 7KM2112-0BA00-3AA0


 Registrierung notwendig  PAC3200lp2_V2_4_3.zip (11,4 KB)

Security information
In order to protect technical infrastructures, systems, machines and networks against cyber threats, it is necessary to implement – and continuously maintain – a holistic, state-of-the-art IT security concept. Siemens’ products and solutions constitute one element of such a concept. For more information about cyber security, please visit
https://www.siemens.com/cybersecurity#Ouraspiration.