×
Siemens Industry Online Support
Siemens AG
Entry type: Product note Entry ID: 31981855, Entry date: 10/20/2008
(1)
Rate

Discontinuation of the complete SIJECT range of products

  • Entry
  • Associated product(s)

We intend to discontinue the complete range of SIJECT products on Oct. 1, 2009.

We intend to discontinue the complete range of SIJECT products on Oct. 1, 2009. However, spare parts will still be delivered.

A direct successor product for SIJECT CI 16iP is not planned. As a replacement for the existing SIJECT CI 16iP solution, we recommend that you use SIMATIC-based hardware (e.g. MP377 based on WIN AC MP). Existing application solutions based on SIJECT (SIMATIC Step7) can be migrated to new hardware components at a low expenditure.

We recommend that you use "Simotion E510" as I/O module.

We recommend that you migrate to SIMATIC-based hardware for all current and future projects.

We recommend that you migrate to the version "MP377 based on WIN AC MP".

Configuration comparison

Currently used sample solution(without keyboards, list prices valid in October 2008, subject to change without prior notice)

Siject CI 16iP + MP377 12" MLFB (order no.)
MP377 12" 6AV6644-0AA01-2AX0
Siject CI16iP 6AT1131-6DF21-0AB0

The following configuration should be preferably used for migration (without keyboards, subject to change without prior notice):

MP377 Bundle 12"  
Simotion E510 6AU1510-6XX00-1XX0
MP377 Bundle 6AV6652-4FC01-2AA0

A detailed migration concept is available on request from the local Siemens sales partners.

Security information
In order to protect technical infrastructures, systems, machines and networks against cyber threats, it is necessary to implement – and continuously maintain – a holistic, state-of-the-art IT security concept. Siemens’ products and solutions constitute one element of such a concept. For more information about cyber security, please visit
https://www.siemens.com/cybersecurity#Ouraspiration.
Rate entry
no rating
Requests and feedback
What do you want to do?
Note: The feedback always relates to the current entry / product. Your message will be forwarded to our technical editors working in the Online Support. In a few days, you will receive a response if your feedback requires one. If we have no further questions, you will not hear from us.