×
Siemens Industry Online Support
Siemens AG
Entry type: Product note Entry ID: 32011372, Entry date: 10/20/2008
(0)
Rate

Service Pack 1 for SIMATIC iMap V3.0

  • Entry
  • Associated product(s)

Service Pack 1 (SP1) for SIMATIC iMap V3.0 has been released and is available for free downloading from the Internet (entry 32011522).

Service Pack 1 provides users of SIMATIC iMap V3.0 with the ability to use components created with the SIMATIC iMap STEP 7 Add-On V3.0 SP4, in SIMATIC iMap. This will permit integration of additional devices in SIMATIC iMap V3.0.

What’s NEW in Service Pack 1?

SIMATIC iMap V3.0 SP1 provides the following new features for configuration, commissioning and testing of systems:

  • Composed data types which can include additional composed data types, e.g. multidimensional arrays and structures of arrays and structures, are supported for devices with PROFINET runtime version V2.3 and higher.
    Creation of PROFINET interfaces and PROFINET components of such devices is supported by SIMATIC iMap STEP 7 Add-On V3.0 SP4 and higher.
  • The maintenance status of PROFINET devices with PROFINET runtime version V2.3 and higher is displayed in symbolics in the online view.
  • SIMATIC iMap will now execute under MS Windows Vista.
  • Version numbers for functions can be specified when creating the PROFINET component and will be displayed in SIMATIC iMap in the features of the PROFINET component.
  • Generation of PROFINET devices without Proxy functionality can be accelerated, if desired.
  • Typical values and absolute limiting values for the performance and loading parameters will be indicated for devices with PROFINET runtime version V2.3 and higher.

 

  • More information on Service Pack 1 for SIMATIC iMap V3.0 is available from the readme file

How can the Service Pack be obtained? 

  • Download
    As usual, we are offering a free download. See entry 32011522.

 

Installation prerequisites for the Service Pack:

The Service Pack can be installed directly over the existing SIMATIC iMap V3.0.

 

To be able to use the new functionality you require the SIMATIC iMap STEP 7 Add-On V3.0 SP4 (see entry ID 32010633).

 

Security information
In order to protect technical infrastructures, systems, machines and networks against cyber threats, it is necessary to implement – and continuously maintain – a holistic, state-of-the-art IT security concept. Siemens’ products and solutions constitute one element of such a concept. For more information about cyber security, please visit
https://www.siemens.com/cybersecurity#Ouraspiration.