×
Siemens Industry Online Support
Siemens AG
Entry type: FAQ, Entry ID: 32049393, Entry date: 10/29/2008
(0)
Rate

Important notes on the documentation for PCS 7 V7.0 SP1

  • Entry
  • Associated product(s)

Description:
An error has been discovered in the PCS 7 documentation.
In the manual "Product Brief on Software Updates from V5.1/V5.2 to PCS 7 V7.0 SP1", chapter 6 "Guide - Basic Procedure for Updating Software", step 23 states that the Project Migrator is only to be run in the case of a software update with new functions. This step must also be carried out in software updates without new functions.


Fig. 01

Security information
In order to protect plants, systems, machines and networks against cyber threats, it is necessary to implement – and continuously maintain – a holistic, state-of-the-art industrial security concept. Siemens’ products and solutions constitute one element of such a concept. For more information about industrial security, please visit
http://www.siemens.com/industrialsecurity.