Entry type: FAQ, Entry ID: 32118459, Entry date: 11/06/2008
(0)
Rate

Which diagnostics messages might you get when commissioning the ET 200S as PROFINET IO device?

  • Entry
  • Associated product(s)

Description:
This entry provides you with information on possible diagnostics messages you might get when commissioning an ET 200S as PROFINET IO device.

Proceed as follows to determine the diagnostics message.

  • In the SIMATIC Manager, you open the menu "PLC > Show Accessible Nodes" to diagnose the separate nodes of the PROFINET IO system.
  • Right-click the PROFINET IO device you wish to diagnose and select the menu "PLC -> Module status".
  • The "Module Status" dialog opens.
  • In the "IO Device Diagnostics" tab you see the standard diagnostics message of the PROFINET IO device which you might get during commissioning.

The following standard diagnostics message indicates that there is not termination module slotted in the ET 200S. You also get this standard diagnostics message when more than one module of the ET 200S station has been removed.


Fig. 01: Termination module not slotted or more than one module of the ET 200S station removed

The standard diagnostics message "Module missing..." indicates that a module in the ET 200S has been removed. Check whether a module is slotted in the specified slot in the ET 200S station.


Fig. 02: A module of the ET 200S station removed

The standard diagnostics message "Incorrect module..." indicates that a different module to the one slotted in the ET 200S has been configured. Check in the STEP 7 hardware configuration whether the module you have configured for the slot specified is the one that is slotted in that slot in the ET 200S station.


Fig. 03: Incorrect module configured 

The following table gives you an overview of the STATUS of SF and BF LEDs when you get one of the above-mentioned standard diagnostics messages.
 

Diagnostics message SF BF
Termination module not slotted (when starting up the ET 200S station) Off Flashes
More than one module of the ET 200S station removed Lights continuously Flashes
One module of the ET 200S station removed Lights continuously Off
Incorrect module configured  Lights continuously Off

Error details
Detailed error description
Help us to improve Online Support.
The page requested cannot be displayed. Please contact the webmaster.
Contact to webmaster