×
Siemens Industry Online Support
Siemens AG
Entry type: Application example Entry ID: 32201967, Entry date: 12/16/2008
(1)
Rate

SIMATIC Route Control - Control of material transports with Route Control using the example of a project extension

  • Entry
  • Associated product(s)

 

Purpose of this document
This application shall provide an overview of what steps have to be taken when an existing PCS 7 project is to be extended by SIMATIC Route Control.

Main contents
The following main points are discussed in this application:

  • Extending the configuration in SIMATIC Manager
  • Engineering with SIMATIC Route Control

Downloads

Inhalt der Downloads Download
SIMATIC Route Control
Control of material transports with Route Control using the example of a project extension
32201967_ApplicationNote_RouteControl_en.pdf ( 1119 KB )

 

History

Version

Modification

11/2008 V1.0

First Release

12/2008 V1.1 Correction Figure 2-1

 

Security information
In order to protect technical infrastructures, systems, machines and networks against cyber threats, it is necessary to implement – and continuously maintain – a holistic, state-of-the-art IT security concept. Siemens’ products and solutions constitute one element of such a concept. For more information about cyber security, please visit
http://www.siemens.com/industrialsecurity.