×
Siemens Industry Online Support
Siemens AG
Entry type: FAQ Entry ID: 32447942, Entry date: 08/23/2010
(0)
Rate

How do you configure a VPN tunnel between a PC station and SCALANCE S61x via the Internet with the 2008 edition of SOFTNET Security Client?

  • Entry
  • Associated product(s)

Description:
From the 2008 edition of SOFTNET Security Client (SSC), you can establish a VPN tunnel with a SCALANCE S61x via the Internet by means of pure configuration with the Security Configuration Tool (SCT). The SCALANCE S 61x is operated in routing mode.


Fig. 01

Please follow the instructions below for configuring the VPN tunnel.

32447942_VPN_Tunnel_Internet2_e.pdf ( 1168 KB )

Note:
If, in addition, you have activated one or more firewalls in this configuration (see Fig. 01), then ports 500 and 4500 of the firewall must be enabled.

Important:
This constellation has been tested on several standard PCs in Windows XP SP2. However, we cannot guarantee that this example will work properly in all PC configurations.

Security information
In order to protect technical infrastructures, systems, machines and networks against cyber threats, it is necessary to implement – and continuously maintain – a holistic, state-of-the-art IT security concept. Siemens’ products and solutions constitute one element of such a concept. For more information about cyber security, please visit
http://www.siemens.com/industrialsecurity.