×
Siemens Industry Online Support
Siemens AG
Entry type: Download Entry ID: 32469496, Entry date: 04/05/2019
(11)
Rate

S7-PCT V3.5 SP1 for IO-Link Master

  • Entry
  • Associated product(s)
The Port Configuration Tool ("PCT") is a PC-based software for parameterizing Siemens IO-Link master modules and third-party IO-Link devices.

The IO-Link devices are integrated using the standardized device description "IODD" which can be obtained from the relevant device manufacturer. S7-PCT supports both IODD versions 1.0 and V1.1.
All IO-Link devices available to Siemens are already available in the hardware selection catalog of S7-PCT.
S7-PCT is called up via the IO-Link master hardware configuration of STEP 7, but it can also be started in "standalone" mode if the IO-Link master is not operated on a SIMATIC controller or no STEP 7 is used.
You can find additional information on the IO-LINK on the Internet at:

http://www.siemens.com/IO-Link

 

New functions in PCT version V3.5 SP1:

The following new functions have been added compared to the previous version 3.5 Upd1:

  • Support of IO-Link Master module for S7-1500 / ET 200MP
  • Firmware update function for IO-Link devices




Supported IO-Link masters:
The following IO-Link masters can be configured with S7-PCT V3.5 SP1:

Product familyDesignationIncluding firmware
version
Article numberManual
SIMATIC S7-1500 /ET 200MP CM8xIO-Link V1.06ES7 547-1JF00-0AB0 109763143 
SIMATIC S7-1200SM1278 4xIO-Link Master ModulesV2.0

6ES7278-4BD32-0XB0


107623221
ET 200SPCM 4xIO-LinkV2.2

6ES7137-6BD00-0BA0

67328527
ET 200S4SI IO-LinkV1.06ES7138-4GA50-0AB0 29825814
ET 200S4SI SIRIUSV1.03RK1005-0LB00-0AA0 37856470
ET 200eco PN

IO-LINK MASTER

4IO-L + 8DI + 4DO DC 24V/1.3A 8 X M12

V7.06ES7148-6JA00-0AB0 29999018
ET  200eco PN

IO-LINK MASTER 4 IO-L, 4xM12

V1.16ES7148-6JD00-0AB029999018 
ET 200ALCM 4X IO-LINKV1.16ES7147-5JD00-0BA0 89254868
ET 200pro4 IO-LINK HIGH FEATUREV1.16ES7147-4JD00-0AB0109738534 

Installation requirements:
S7-PCT V3.5 is a 32-bit application which has been released for use with the following operating systems:
MS Windows 7 SP1 64-bit Ultimate, Professional and Enterprise
• MS Windows 8.1 64-bit Professional and Enterprise
• MS Windows 10, 64-bit Home, Professional and Enterprise

• MS Windows Server 2008 R2 StdE SP1 64-bit
• MS Windows Server 2012 R2 StdE 64-bit
• MS Windows Server 2016 64-bit

There is no guarantee that S7-PCT V3.5 SP1 will run on other operating systems. The user does so at their own risk.

Download:
Before downloading the S7-PCT setup, read the "Readme.rtf"
 Registrierung notwendig  S7-PCT_V3.5_SP1_Readme.zip (998.9 KB)

S7 PCT V3.5 SP1 Setup
 Registrierung notwendig  S7-PCT_V3.5_SP1.zip (362.8 MB)

Security information
In order to protect technical infrastructures, systems, machines and networks against cyber threats, it is necessary to implement – and continuously maintain – a holistic, state-of-the-art IT security concept. Siemens’ products and solutions constitute one element of such a concept. For more information about cyber security, please visit
https://www.siemens.com/cybersecurity#Ouraspiration.