×
Siemens Industry Online Support
Siemens AG
Entry type: FAQ Entry ID: 32582476, Entry date: 04/04/2016
(0)
Rate

MICROMASTER 4 (MM4): Transfering projects from DriveMonitor into STARTER

  • Entry
  • Associated product(s)
MICROMASTER 4 drive inverters can be parameterized using the DriveMonitor and STARTER commissioning tools.


How can I transfer projects from DriveMonitor into STARTER?

In order to transfer the values saved in DriveMonitor into STARTER, several steps are necessary, that will be presented using as an example a MICROMASTER 440.

Information attached


  pdf_projects_drivemonitor_to_starter_en_v2.pdf (693,2 KB) 

 Registrierung notwendig  executednl.zip (1 KB)

Security information
In order to protect technical infrastructures, systems, machines and networks against cyber threats, it is necessary to implement – and continuously maintain – a holistic, state-of-the-art IT security concept. Siemens’ products and solutions constitute one element of such a concept. For more information about cyber security, please visit
https://www.siemens.com/cybersecurity#Ouraspiration.