×
Siemens Industry Online Support
Siemens AG
Entry type: Download Entry ID: 33124038, Entry date: 07/29/2013
(3)
Rate

SINAMICS S120 Firmware Version 2.6 SP2 HF19

  • Entry
  • Associated product(s)
Here you can find the SINAMICS S120 Firmware Version 2.6 SP2 HF19.
Description

The version designation on the memory card (CF) is SINAMICS S120 V02.06.02.19.
The internal firmware version number is SINAMICS S120 V02.60.45.31.

When upgrading your system, please read the firmware update instructions.

 

Restrictions for SINAMICS S120
  sinamics_v2_6_sp2_restrictions.pdf (38,3 KB)

 

Functional restrictions for SINAMICS S120 CU320 and CU310  which have been corrected
  corrected_functional_restrictions_s120_v26_sp2_hf19.pdf (37,1 KB)

 

Firmware update instructions regarding SINAMICS S120 CU320 and CU310
When upgrading, please read the instructions regarding the firmware update:
  instruction_firmware_update_sinamics_s120.pdf (174,8 KB)

 

SINAMICS S120 firmware version 2.6 SP2 HF19 for CU320 and CU310

The following software can be downloaded:

Note:
The software is subject to export restrictions.
The download is only available to registered users.

Due to export regulations a download is only possible within the EU.

 
Alternatively you can use a new memory card (CF) with the following order number for upgrading:

  • without performance extension:
    Order no. 6SL3054-0CG00-1AA0
  • with firmware option performance extension:
    Order no. 6SL3054-0CG01-1AA0

 

Faults and warning lists
"Alarmlist_*.xml" files are not required to properly operate the firmware and related STARTER. They only contain a text extract of the S120 "alarm messages" in "xml" format (this format ensures that the text is displayed correctly independently of worldwidediffering  fonts and can thus be correctly converted into other formats).
In some cases, this text extract is required by customers who wish to further use it in their applications resp. integrate it in external units. For this reason, we cannot provide any further support for the S120.

  alarmlist_s_v02603900_chs.xml (1,8 MB)
  alarmlist_s_v02603900_eng.xml (1,9 MB)
  alarmlist_s_v02603900_esp.xml (2,0 MB)
  alarmlist_s_v02603900_fra.xml (2,0 MB)
  alarmlist_s_v02603900_ita.xml (2,0 MB)
  alarmlist_s_v02604100_deu.xml (1,9 MB)

 

GSD-files for usage in PROFIBUS configuration tools
The PROFIBUS GSD files are stored on the SINAMICS S120 Compact Flash Card under the following path: 
..\SIEMENS\SINAMICS\DATA\CFG

 

EDS-files for usage in CANopen configuration tools
see 48802094

 

STARTER
STARTER Version ≥ 4.1.3 is required for this Firmware Version  (see Entry 26233208)

and the appropriate SSP for SINAMICS V2.6 SP2.
(see Entry 39700146)

 

DCC (Drive Control Chart)
New orders:
DCC-SINAMICS V2.0 SP5 is supplied on a data medium (DVD) and the related engineering floating license (on USB stick).
DCC comprises a graphic configuring tool (DCC Editor/CFC) and the block library (DCB library). DCC is installed in addition to the engineering software SCOUT resp. STARTER. When ordering DCC, you also purchase the engineering license required for each PC (floating) for DCC. Additional runtime licenses are not required.
  • DCC-SINAMICS V2.0 SP5 (6AU1810-1HA20-5XA0):
    Single engineering license, with data medium DCC. DCC Editor + DCB library for use on SINAMICS S120 V2.6 SP2.
Upgrade from DCC V2.0 to DCC V2.0 SP5:
A new order need not be placed for already existing DCC licenses of an older V2.0 version (e.g. for SINAMICS V2.5.x).
The license V2.0 still remains valid for V2.0 SP5 as well.
The "new" software package DCC V2.0 SP5 is also included in the setup of STARTER or SCOUT V4.1 SP3 resp. the corresponding SSPs (libraries and CFC Editor; the CFC Editor must be explicitly selected upon setup) and can thus also be installed from there without purchasing the DCC-DVD. It is not necessary to separately install (or order, if license already exists) the DCC-DVD.
 

"Testing" DCC without placing an order:
DCC can be used without limitations during 14 days without the engineering floating license.
For this, install the DCC - as described under "upgrade" - via the STARTER or SCOUT setup. The related TRIAL license (14 days) is available for this.

 

Security information
In order to protect technical infrastructures, systems, machines and networks against cyber threats, it is necessary to implement – and continuously maintain – a holistic, state-of-the-art IT security concept. Siemens’ products and solutions constitute one element of such a concept. For more information about cyber security, please visit
https://www.siemens.com/cybersecurity#Ouraspiration.