×
Siemens Industry Online Support
Siemens AG
Entry type: Product note Entry ID: 33400780, Entry date: 12/22/2008
(0)
Rate

Compatibility of WinAC RTX on PCs with Single-Core Microprocessors

  • Entry
  • Associated product(s)

To be able to operate WinAC RTX 2005 or 2008 on Single-Core microprocessors without Hyperthreading or with Hyperthreading switched off, you require a "ACPI Uniprocessor" HAL to be able to completely install WinAC RTX.

Description

If you wish to install WinAC RTX on a Single-Core microprocessor with installed Multiprocessor HAL and running without Hyperthreading or with Hyperthreading switched off , WinAC RTX will abort installation with the error message "Unable to install RTX ... Runtime on this system ...". In this case you must first install a suitable "ACPI Uniprocessor PC" HAL before you can install WinAC RTX.

Correction

An FAQ is available for the current SIMATIC PCs

  • SIMATIC Box PC
  • SIMATIC RACK PC
  • SIMATIC Panel PC:

under "Why does the installation of WinAC RTX 2005 (SP1) RTX 6.5.1 abort?" with hints on how to correct the problem:

 http://support.automation.siemens.com/WW/view/en/28947641

The description provided here for WinAC RTX 2005 is correspondingly valid for WinAC RTX 2008 with Ardence RTX V8.1.

For other PCs please proceed as follows:

  • Please check whether the "ACPI Uniprocessor" HAL is available on your PC. You will find the installed HAL type in the Windows Device Manager under "Computer".
  • Contact your PC manufacturer whether he can supply a matching ACPI Uniprocessor HAL or whether it is available on this system.
  • Install the Uniprocessor HAL according to the manufacturer’s instructions.

Security information
In order to protect technical infrastructures, systems, machines and networks against cyber threats, it is necessary to implement – and continuously maintain – a holistic, state-of-the-art IT security concept. Siemens’ products and solutions constitute one element of such a concept. For more information about cyber security, please visit
https://www.siemens.com/cybersecurity#Ouraspiration.
Requests and feedback
What do you want to do?
Note: The feedback always relates to the current entry / product. Your message will be forwarded to our technical editors working in the Online Support. In a few days, you will receive a response if your feedback requires one. If we have no further questions, you will not hear from us.
Support to the statistics
With this function the IDs found are listed according to number (format .txt).

Generate list
Copy URL
Display page in new design
mySupport Cockpit