×
Siemens Industry Online Support
Siemens AG
Entry type: FAQ Entry ID: 34010717, Entry date: 10/04/2017
(11)
Rate

Which ports are released for Modbus/TCP communication and how many Modbus clients can communicate with a SIMATIC S7 PN-CPU as Modbus server?

  • Entry
  • Associated product(s)
Ports released for Modbus/TCP communication and maximum number of Modbus clients that can communicate with a SIMATIC S7 PN-CPU as Modbus server

The following ports are used by the Modbus/TCP protocol.

  • By default, the protocol uses Port 502 as local port in the Modbus server.
  • You can set the local port as you wish in the Modbus client. Usually, port numbers starting at 2000 are used.

If the communication partners offer the option of setting the port numbers for the server, then it is also possible to communicate using the Modbus/TCP protocol via a port other than Port 502.

If you use the SIMATIC as Modbus server, then there are restrictions for a number of CPUs regarding the released port numbers.
The following port numbers are released for the local port.
 
 34010717_CPU_ModbusServer_en.pdf (7,9 KB)
  

If you use the SIMATIC CPU as Modbus client, then there are no restrictions regarding the released port numbers. You can set any remote port of the CPU.

Number of possible communication connections using Modbus/TCP protocol
The maximum number of Modbus clients that can be connected to one S7-300 or S7-400 CPU with integrated PROFINET interface is limited by the CPU-specific quantity frameworks.
Maximum 8 Modbus clients can be connected to one S7-1200 CPU.
The maximum number of Modbus clients that can be connected to one S7-1500 CPU is determined by the number of MB_Server FB instances running in parallel on the CPU and the maximum number of free connection resources.
If the CPU with integrated PROFINET interface does not support multiple ports, each local port of the CPU can only be used once, which means that when a communication connection has been established for one local port of the CPU, then you cannot set up another connection via that port.
If a non-multiport CPU is used as Modbus server, then there are two options for establishing communication connections to multiple Modbus clients.

  • You parameterize different port numbers for the Modbus server in the Modbus client.



Fig. 01
  
  • All Modbus clients access the Modbus server via Port 502.
    In this case, it is necessary to have constant job-controlled establishment and clear-down of connections. The Modbus server can communicate with only 1 Modbus client through Port 502 at any one time. The connection to the first Modbus client must be cleared down and Port 502 released before another Modbus client can access the Modbus server. As soon as Port 502 is released, another Modbus client can access the Modbus server via that port.
     

Case 01


Fig. 02
  

Case 02


Fig. 03
 


Fig. 04
 


Fig. 05
 

Further Information
More information about multiport-compatibility is available in the technical data of the CPU.
If the CPU supports multiple passive connections per port for open IE communication, it is multiport-compatible.
 

ManualEntry ID
SIMATIC S7-300 CPU 31xC and CPU 31x: Technical Data

12996906

SIMATIC Distributed IO ET 200S Interface Module IM151-8 PN/DP CPU

47409312

Automation System SIMATIC S7-400 CPU Specifications

53385241

SIMATIC S7-1200 Automation System

36932465

SIMATIC S7-1500, ET 200MP, ET 200SP, ET 200AL Communication59192925
How do you process asynchronous instructions with the S7-1500?109476955
Table 1



Security information
In order to protect technical infrastructures, systems, machines and networks against cyber threats, it is necessary to implement – and continuously maintain – a holistic, state-of-the-art IT security concept. Siemens’ products and solutions constitute one element of such a concept. For more information about cyber security, please visit
https://www.siemens.com/cybersecurity#Ouraspiration.