×
Siemens Industry Online Support
Siemens AG
Entry type: Product note Entry ID: 34102366, Entry date: 01/29/2009
(0)
Rate

Introduction of software, order option W01 and W02 for service packs in conjunction with SIMOTION P350-3

  • Entry
  • Associated product(s)

From the introduction of SIMOTION V4.1 SP2 HF3/4, two new options - W01 and W02 - have been introduced. These options must always be specified in addition to version option V41 as otherwise the order will not be accepted.

The introduction of the option was necessary in order that a special service pack software release can be ordered. This means that it is not necessary to change over the runtime software of the SIMOTION P350.  Previously, when ordering, only the software version without service pack was able to be specified. The fact that a service pack can be ordered means that it is necessary to specify the service pack when ordering.

W01 option for service pack 1
W02 option for service pack 2

This applies for the following Order Nos. [MLFBs]

6AU1350-3AK41-1BE2 SIMOTION P350-3 with PROFIBUS without DVD
6AU1350-3AK43-1BE2 SIMOTION P350-3 with PROFIBUS with DVD

6AU1350-3AK41-2BE2 SIMOTION P350-3 with PROFINET without DVD
6AU1350-3AK43-2BE2 SIMOTION P350-3 with PROFINET with DVD

Ordering examples:

  • 6AU1350-3AK41-2BE2 -Z V41 W01    SIMOTION P350 with RT software 4.1 SP1 HF6 installed
  • 6AU1350-3AK41-2BE2 -Z V41 W02    SIMOTION P350 with RT software 4.1 SP2 HF3 installed

Note:
The order option for the service pack is only valid from software version V4.1 and higher (optionV41) and is not possible for option V40.

Security information
In order to protect technical infrastructures, systems, machines and networks against cyber threats, it is necessary to implement – and continuously maintain – a holistic, state-of-the-art IT security concept. Siemens’ products and solutions constitute one element of such a concept. For more information about cyber security, please visit
https://www.siemens.com/cybersecurity#Ouraspiration.
Rate entry
no rating
Requests and feedback
What do you want to do?
Note: The feedback always relates to the current entry / product. Your message will be forwarded to our technical editors working in the Online Support. In a few days, you will receive a response if your feedback requires one. If we have no further questions, you will not hear from us.