×
Siemens Industry Online Support
Siemens AG
Entry type: FAQ Entry ID: 34128511, Entry date: 04/15/2013
(2)
Rate

Alignment, alignment values, alignment methods, alignment in relation to thermal growth, alignment in relation to journal bearings, alignment tool

  • Entry
  • Associated product(s)

 

QUESTION:

 

 

 

 

 

What type of damage can be caused by incorrect alignment?

Which four values are used when aligning a machine?

What alignment methods are available?

What needs to be considered when performing alignment in relation to thermal growth and journal bearings? Which alignment tool is used?


ANSWER / REMEDY / NOTES:

  

 

 

 

 

Incorrect alignment of machines can cause premature damage and reduce their service life:

 

 

  • Bearing

  • Coupling

  • Seal

  • Shaft

 

 

   

Motor damage as a result of incorrect alignment

     
     
    Four alignment values
     
   
     
     
    Alignment methods
     
   
     
     
    Alignment in relation to thermal growth
     
   

This alignment method is generally used for cold machines. In the case of larger machines and those where different steady-state temperatures occur for the motor and the driven machine, the effects of thermal growth on machine alignment should be taken into account.

     
   
     
    Effects of thermal machine growth on alignment quality
     
   

In the case of large machines, details of thermal growth are provided in the machine manual. Approximate calculations can be performed if the manufacturer does not provide any information:

     
   

DL = L x a x DT

     
   

DL

L

a

DT

Thermal growth

Center-line height for machine foundation plate

Coefficient for thermal growth (e.g. 0.0000059 for cast iron)

Expected temperature change

     
     
    Alignment in relation to journal bearings
     
   

A motor shaft featuring journal bearings with no oil pressure relief is displaced both upwards and sideways during operation, depending on the oil film.

The level of displacement is approx. 0.05 mm in both directions for oils with viscosity class VG 46. This value increases if oils with a higher viscosity class are used. If machine sets are only operated in one direction of rotation, care should be taken when aligning this shaft displacement to avoid twisting or even inflicting damage on the driven machine's rolling-contact bearings.

     
   

Top view

 

Direction of

rotation

Side view

   

1) Service position of shaft in journal bearings

2) Rest position of shaft in journal bearings

a) Shaft with journal bearings

b) Shaft with rolling-contact bearings

c) Vertical displacement of shaft a during operation c) Horizontal displacement of shaft a during operation

     
     
    Alignment tool
   

 

 

 

 

 

     

 

Security information
In order to protect technical infrastructures, systems, machines and networks against cyber threats, it is necessary to implement – and continuously maintain – a holistic, state-of-the-art IT security concept. Siemens’ products and solutions constitute one element of such a concept. For more information about cyber security, please visit
https://www.siemens.com/cybersecurity#Ouraspiration.