×
Siemens Industry Online Support
Siemens AG
Type de contribution : FAQ ID de la contribution : 34388051, Date de la contribution : 05/02/2009
(1)
Évaluer

Mechanical distortion after installation - "soft foot"

  • Contribution
  • Concerne le/les produits(s)

 

QUESTION:

 

 

 

 

 

What is soft foot and how is it possible to find out if it exists?


ANSWER / REMEDY / NOTES:

  

 

 

 

 

If motors are installed in such a way that they are subjected to mechanically distorting forces, increased vibration or noise can be the consequence. The most common cause of distorted motor housings is the so-called "soft foot" problem.

 

 

 
   
     
   

There is an easy way to detect housing distortion due to soft foot:

This is done by loosening the bolted connections of the four motor feet one after the other, one foot at a time. After loosening a foot while leaving the other three feet firmly tightened, the procedure is as follows and must be repeated for each foot:

A dial indicator is attached to the motor foot. If changes in the vertical position of the motor foot are indicated when the bolted connection is loosened, the motor housing is distorted due to soft foot.

If soft foot is detected when the motor is being aligned, it must be corrected by inserting or removing shims under the feet.

In the case of angular soft foot, step shims may be necessary. Unless indicated otherwise by the manufacturer, the amount of soft foot should not be more than 0.05 mm.

     

Notes relatives à la sécurité
La protection des installations, systèmes, machines et réseaux contre les cyber-menaces nécessite la réalisation (et le maintien continu) d'un concept global de sécurité IT à la pointe de la technique. Les produits et solutions Siemens ne constituent qu'un élément d'un tel concept. Pour plus d’informations sur la cyber-sécurité, rendez-vous sur
https://www.siemens.com/cybersecurity#Ouraspiration.
Aide pour la statistique
Cette fonction permet de délivrer les identifiants des résultats de la recherche selon la quantité souhaitée (format .txt).

Générer une liste
Copier l'URL
Afficher cette page dans le nouveau design
Poste de commande mySupport
Liens connexes