×
Siemens Industry Online Support
Siemens AG
Entry type: Download Entry ID: 35029840, Entry date: 09/01/2021
(10)
Rate

Firmware Update Measuring Device 7KM PAC4200

  • Entry
  • Associated product(s)
Downloads Firmware Update Measuring Device 7KM PAC4200 for products: 7KM4212-0BA00-3AA0, 7KM4212-0BA00-2AA0, 7KM4211-1BA00-3AA0 ...

Description:

If the device firmware is updated, the respective firmware always has to be updated to the latest version available for the PAC4200. Please note that a firmware update may also require a new version of the language package.

The update can be peformed by application of the configuration software SENTRON powerconfig, which is available in the internet.

A description of the update procedure can be found in the online help of the software.

Newest version:

Update V2.3.3
(7KM4212-0BA00-3AA0, 7KM4212-0BA00-2AA0, 7KM4211-1BA00-3AA0)

The firmware update V2.3.3 incorporates the following modification: 

  • Increase in cyber security.

Note! 
  • After updating to the firmware version V2.3.3, an older version (<V2.3.3) must not be loaded because this would lead to an irreversible malfunction of the device.
  • After updating the PAC 4200 to firmware V2.3.3 it is not necessary to update a new language package. 
  • The use of the latest Powerconfig version is very important.

Third-party software - Licensing terms and copyright information

You can find the copyright information for third-party software contained in this product, particularly open source software, as well as applicable licensing terms of such third-party software in the Readme_OSS file.

Special information for resellers

The information and the license terms in the Readme_OSS file must be passed on to the purchasing party to avoid license infringements by the reseller or purchasing party.


DOWNLOAD:

Application firmware version: V2.3.3 (07/2021)
PAC4200, 7KM4212-0BA00-3AA0, 7KM4212-0BA00-2AA0, 7KM4211-1BA00-3AA0

 Download unterliegt Exportcontrolle  PAC4200fw_V2.3.3-0.0.1.0.fwp.zip (484,2 KB)(SHA-256)

Information about SHA-256 109483101 



Older version:

Update V2.3.0
(7KM4212-0BA00-3AA0, 7KM4212-0BA00-2AA0, 7KM4211-1BA00-3AA0)

The firmware update V2.3.0 incorporates the following modification:

  • The web server has been improved to avoid sending corrupt data
  • Ethernet driver enhanced for better data throughput, higher stability and more balanced cou load
  • Handling of SNTP-IP in DATE / TIME parameter screen (V2.2.x only bug) fixed
  • Scaling factor in screen 7.0 fixed
  • Erroneous popups "SEAbus TCP" and overvoltage signaling at startup fixed
  • Fix wrong screen title for "VOLTAGE INPUTS" in SETTINGS -> BASIC PARAMETERS
  • Hide screen "Voltage Vph-n" and "Harm. Voltage Vph-n" in case of hookup 3P3WB, 3P3W
  • Behaviour of Battery change screen fixed (V2.2.x only bug)
  • Fix value range in SETTINGS -> DISPLAY -> CONTRAST to 0..10 (V2.2.x: 1..10)
  • Fix uIP vulnerabilities

Note!

  • After updating to the firmware version V2.3.0, an older version (<V2.3.0) must not be loaded because this would lead to an irreversible malfunction of the device.
  • After updating the PAC 4200 to firmware V2.3.0 it is not necessary to update a new language package. 
  • The use of the latest Powerconfig version is very important


Update V2.2.5
(7KM4212-0BA00-3AA0, 7KM4212-0BA00-2AA0, 7KM4211-1BA00-3AA0)

The firmware update V2.2.5 incorporates the following modification:

  • Update PSS-Sigcont for signed firmware update to recent version
  • Add support for Gratuitous ARP for VLAN authentication
  • Registermapping of aggregation files enhanced in order to get I4, I5, I6 Indiff-Module values

Note!

  • After updating to the firmware version V2.2.5, an older version (<V2.2.5) must not be loaded because this would lead to an irreversible malfunction of the device.
  • After updating the PAC 4200 to firmware V2.2.5 it is not necessary to update a new language package. 
  • The use of the latest Powerconfig version is very important
Update V2.2.4
(7KM4212-0BA00-3AA0, 7KM4212-0BA00-2AA0, 7KM4211-1BA00-3AA0)

The firmware update V.2.2.4 incorporates small modifications

Note!

  • After updating to the firmware version V2.2.4, an older version (<V2.2.4) must not be loaded because this would lead to an irreversible malfunction of the device
  • After updating the PAC 4200 to firmware V2.2.4 it is not necessary to update a new language package
  • The use of the latest Powerconfig version is very important
Update V2.2.1
(7KM4212-0BA00-3AA0, 7KM4212-0BA00-2AA0, 7KM4211-1BA00-3AA0)

The firmware update V2.2.1 incorporates the following modification:

  •  Integration Web Server

Note!

  • After updating to the firmware version V2.2.1, an older version (<V2.2.1) must not be loaded because this would lead to an irreversible malfunction of the device.
  • After updating the PAC 4200 to firmware V2.2.1 it is not necessary to update a new language package. 
  • When updating devices with FW <2.0.0, an intermediate step is always neccessary. This intermediate step is automatically carried out during the firmware update and can thus be upgraded directly to the new future versions >V2.0.0.
Update V2.0.1
(7KM4212-0BA00-3AA0, 7KM4212-0BA00-2AA0, 7KM4211-1BA00-3AA0)

The firmware update V2.0.1 incorporates the following modification: Small optimizations.

Note!

  • After updating to the firmware version V2.0.1, an older version (<V2.0.1) must not be loaded because this would lead to an irreversible malfunction of the device.
  • After updating the PAC 3200 to firmware V2.4.5 it is not necessary to update a new language package. 
  • If PAC4200 Devices with Versions < V2.0.0 should be updated to Versions > V2.0.0 (e.g. V1.6.1 to V2.1.x), V2.0.0 is needed first! From this FW V2.0.0 can then be upgraded directly to the new future versions> V2.0.0.
Update V2.0.0
(7KM4212-0BA00-3AA0, 7KM4212-0BA00-2AA0, 7KM4211-1BA00-3AA0)

The firmware update V2.0.0 incorporates the following modification:

  • Extensions regarding IT scurity (signed firmware, penalty time, new IP filter, configurable IP Ports)
  • HW write protection settable via local HMI
  • DHCP Client
  • Parameterizable default screen
  • Aggregation Logs: Data over time averaged values.
  • More Harmonics: All Harmonics 1,2,3 ... 64 can be reported.

Note!

  • After updating the PAC4200 to firmware V2.0.0 it is imperative to update the language package to version V2.0.0! The related language package can also be found on this download page.
  • If PAC4200 Devices with Versions <V2.0.0 should be updated to Versions > V2.0.0 (e.g. V1.6.1 to V2.1.x), V2.0.0 is needed first! From this FW V2.0.0 can then be upgraded directly to the new future versions > V2.0.0.
  • After updating to the firmware version V2.0.0, an older version (<V.2.0.0) must not be loaded because this would lead to an irreversible malfunction of the device.
Update V1.6.2
(7KM4212-0BA00-3AA0, 7KM4212-0BA00-2AA0, 7KM4211-1BA00-3AA0)

The firmware update V1.6.2 incorporates the following modification: Small optimizations


Note!

  • After updating the PAC4200 to firmware V1.6.2 it is imperative to update the language package to version V1.6.2! The related language package can also be found on this download page.
  • After updating to the firmware version V1.6.2, an older version (<1.6.2) must not be loaded because this would lead to an irreversible malfunction of the device.
Update V1.6.1
(7KM4212-0BA00-3AA0, 7KM4212-0BA00-2AA0, 7KM4211-1BA00-3AA0)

The firmware update V1.6.1 incorporates the following modification:


Note!

  • After updating the PAC4200 to firmware V1.6.1 it is imperative to update the language package to version V1.6.1!
    The related language package can also be found on this download page.
  • After updating to the firmware version V1.6.1, an older version (≤1.6.1) must not be loaded because this would lead to an irreversible malfunction of the device.
Update V1.5.4
(7KM4212-0BA00-3AA0, 7KM4212-0BA00-2AA0, 7KM4211-1BA00-3AA0)

The firmware update V1.5.1 incorporates the following modification:

  • Improvement in the communication behaviour


Note!
 

  • After updating to the firmware version V1.5.4, an older version (≤1.5.4) must not be loaded because this could lead to an irreversible malfunction of the device.
Update V1.5.4
(7KM4212-0BA00-3AA0, 7KM4212-0BA00-2AA0, 7KM4211-1BA00-3AA0)

The firmware update V1.5.1 incorporates the following modification:

  • Ethernet performance optimized
  • Digital in counter enhanced
  • Time sync optimized


Note!

  • After updating the PAC 4200 to firmware V1.5.1 it is not necessary to update a new language package.
  • After updating to the firmware version V1.5.1, an older version (≤1.5.0) must not be loaded because this could lead to an irreversible malfunction of the device
Update V1.5.0
(7KM4212-0BA00-3AA0, 7KM4212-0BA00-2AA0, 7KM4211-1BA00-3AA0)

The firmware update V1.5.0 incorporates the following modification:

  • Extended adjustment range for very big transformer ratios


Note!

  1. After updating the PAC 4200 to firmware V1.5.0 it is imperative to update the language package to version V1.5.0! The related language can also be found on this download page.
  2. After updating to the firmware version V1.5.0, an older version (≤1.5.0) must not be loaded because this would lead to an irreversible malfunction of the device.
Update V1.4.2
(7KM4212-0BA00-3AA0, 7KM4212-0BA00-2AA0, 7KM4211-1BA00-3AA0)

The firmware update V1.4.2 incorporates the following modification:

  • Start-up optimization SRAM + Battery


The above stated version does not contain any new functionalities.


Note!

  1. After updating the PAC 4200 to firmware V1.4.2 it is not necessary to update a new language package.
  2. After updating to the firmware version V1.4.1, an older version (≤1.4.2) must not be loaded because this could lead to an irreversible malfunction of the device.
Update V1.4.1
(7KM4212-0BA00-3AA0, 7KM4212-0BA00-2AA0, 7KM4211-1BA00-3AA0)

This firmware update is strongly recommended for devices with subsequent firmware update to V1.4.0 and a modified setting of the basic parameters (e. g. conversion ratios of transformers), differing from the factory settings.


Firmware update V1.4.1 incorporates the following modifications:

  • Operational improvement of the device when operating with an expansion module PAC 4DI/2DO and simultaneous communication with powermanager or powerconfig in online modus.
  • Amendment of Polish display texts


The above stated version does not contain any new functionalities.


Note!

  1. After updating the PAC4200 to firmware V1.4.1 it is imperative to update the language package to version V1.4.1! The related language package can also be found on the download page of the PAC4200.
  2. After updating to the firmware version V1.4.1, an older version (≤1.4.0) must not be loaded because this could lead to an irreversible malfunction of the device.
Update V1.4.0
(7KM4212-0BA00-3AA0, 7KM4212-0BA00-2AA0, 7KM4211-1BA00-3AA0)

The above-stated version contains the following functional innovations:

  • Full support of the extension modul Switched Ethernet PROFINET (7KM9300-0AE00-0AA0).


Firmware update V1.4.0 incorporates the following modifications:

  • Extented display of decimal places at current and power measurement
  • Improvement of frequency measurement at bad power quality.


Detailed descriptions are available in the customer documentations.
  

Note!

  1. After updating the PAC4200 to firmware V1.4.0 it is imperative to update the language package to version V1.4.0! The related language package can also be found on this download page.
  2. After updating to the firmware version V1.4.0, an older version (≤1.1.x) must not be loaded because this would lead to an irreversible malfunction of the device.
Update V1.3.2
(7KM4212-0BA00-3AA0, 7KM4212-0BA00-2AA0, 7KM4211-1BA00-3AA0)

The above-stated version contains the following functional innovations:

  • Separate new energy- and operation hour counters.
  • Permanent storage of the following data into the flash memory.
    • Total Energy counters for active, reactive and apparent. (active energy for off-peak and on-peak, import and export) ´
    • Partial Energy counters for active, reactive and apparent. (process energy counters)
    • Total time (operating hours counter)
    • Partial time àMachine on process. (process operating hour counter)
    • Device Profile (all setting data but not the time of the real time clock)
    • Historical data (all trends for power - active, reactive and apparent –and cosφ) this includes the load profile memory as it is implemented in the firmware version 1.1.0 additionally the displacement power factor cosj for phase L1, L2 and L3 as instantaneous values at the end of the programmed demand period without min. and max. values


Firmware update V1.3.2 incorporates the following modifications:

  • Incorrect value Usym has been fixed.
  • Event at battery change.
  • Malfunction of parameterization access protection via „Bus“ has been fixed.
  • Parameter setting of events now fail-safe.
  • Malfunction of serial polling of slave has been fixed.
  • Errors at min max values for cos phi are eliminated.
  • Error at Event: "Limit value monitoring" of "process hours counter" has been fixed.
  • Indication error at Connection type 3P3WB.
  • Error in title bar, after deleting a User screen, has been fixed.
  • Unstable IP communication eliminated. (VPN, Internet).
  • Error when deleting the User screens has been fixed.
  • Deleting energy counter by HMI.


Detailed descriptions are available in the customer documentations.


Note!

  1. After updating the PAC4200 to firmware V1.3.2 it is imperative to update the language package to version V1.3.2! The related language package can also be found on this download page.
  2. After updating to the firmware version V1.3.2, an older version (≤1.1.x) must not be loaded because this would lead to an irreversible malfunction of the device.
Update V1.2.0
(7KM4212-0BA00-3AA0, 7KM4212-0BA00-2AA0)

The above-stated version contains the following functional innovations:

  • Event memory
    • An extra “digital input switched on” event will be created for each digital input including the number of the digital input instead of a group signal.
    • A separate event “universal counter deleted” will be logged for each universal counter (1 or 2) instead of a group signal.


Firmware update V1.2.0 incorporates the following modifications:

  • Communication via Gateway
    • The simultaneous and forbidden access of two SW products on any sub device of a PAC4200 will be prohibited to avoid a reboot of the PAC4200.
    • The commands „Reset To Factory Defaults“ or „Reset Device“ for sub devices lead no longer to a reboot of the PAC4200.
    • Sporadically connecting faults to sub devices has been fixed.
  • Parameterization / Commands via communication interfaces
    • Malfunction of tariff switching via „Bus“ has been fixed.
    • Parameter changes on the universal counters will take effect immediately.
    • The usage of the reset command for the daytime energy counters deletes the current value also
    • Switching group „0“ added. Parameterization from 0 to 99 possible.
    • The product version in the I&M data set will be transmitted correctly now.
  • Event memory
    • Outgoing message added for "digital input is ON".
    • Proper return from a detailed view of an event.
    • Event message for operating hour meter added.
  • Digital in- and outputs
    • The wrong assignment between a 2nd, 3rd, … digital input and a free assignable counter (RELATED COUNTER) by using the „COPY&RESET“ or „RESET“ process counter func-tion has been corrected.


Detailed descriptions are available in the customer documentations.


Note!

  1. After updating the PAC4200 to firmware V1.2.0 it is imperative to update the language package to version V1.2.0! The related language package can also be found on this download page.
  2. After updating to the firmware version V1.2.0, an older version (≤1.1.x) must not be loaded be-cause this would lead to an irreversible malfunction of the device.
Update V1.1.0
(7KM4212-0BA00-3AA0, 7KM4212-0BA00-2AA0)

The above-stated version contains the following functional innovations:

  • Support of the SENTRON PAC 4DI/2DO module for expanding the integrated digital inputs and outputs by an additional 4 inputs and 2 outputs per module. A maximum of 2 SENTRON PAC 4DI/2DO modules can be attached to the device.
  • In connection with the SENTRON PAC 4DI/2DO module there are up to 10 counters available for counting the configured actions at the digital inputs.
    • Through the connection of pulse counters it is possible therefore to detect the energy con-sumption of any media such as e.g. gas, water, compressed air, electricity, etc.
    • Through assignment of a counter to several digital inputs it is possible to totalize the weigh-ted pulses of these inputs.
    • The texts in the related device displays are freely definable.
  • Additional counters for apparent, active and reactive energy for detecting the energy con-sumption of a production process or sub-process, including operating hours counters for de-tecting the process duration. These counters are controlled either through the digital inputs on the device or on the PAC 4DI/2DO expansion module. Both the counter readings of the cur-rent process and the readings of the process last completed are indicated.
  • Choice of either a serial gateway for integrating RS485 devices with a protocol similar to Modbus RTU or a pure Modbus gateway with Modbus TCP ↔ Modbus RTU protocol.
  • Second universal counter added.
  • Limit value monitoring of the process hours counter possible.
  • Expansion of the status displays for digital inputs and outputs to include the I/Os of the PAC 4DI/2DO expansion modules as soon as they are taken into operation on the PAC4200.


Firmware update V1.1.0 incorporates the following modifications:

  • Events of the same type are grouped in one popup window, greatly reducing the number of popups needing to be acknowledged. The displayed measured values continue to be updated in the background.
  • Separation of the threshold value for starting the energy counters from the threshold for the operating hours counters. The operating hours counters are given their own, adjustable thres-hold value.
  • Load profile record
  • Sporadic errors in the load profile memory eliminated
  • Popup window supplemented with delete notice for the load profile data in case of relevant parameter changes.
  • Event recording
    • Error with the event "auxiliary voltage failure" corrected
    • Event list expanded to 4096 events
  • Simultaneous resetting of extreme values, counters, universal counters and pulse counters now possible.
  • Incorrect direction data in the reactive power display menu corrected.
  • Calculation of the minimal values during a device start corrected.


Detailed descriptions are available in the customer documentations.


Note!

  1. After updating the PAC4200 to firmware V1.1.0 it is imperative to update the language package to version V1.1.0! The related language package can also be found on this download page.
  2. After updating to the firmware version V1.1.0, an older version (1.0.x) must not be loaded because this would lead to an irreversible malfunction of the device.
Update V1.0.1
(7KM4212-0BA00-3AA0, 7KM4212-0BA00-2AA0)

The above-specified version includes the following functional innovations:

  • Functional support of the SENTRON PAC PROFIBUS DP expansion module with firmware version V3.0.1 and higher (see "Expansion modules -> EXPANSION MODULE PROFIBUS DPV1"; 7KM9300-0AB00-0AA0)


Detailed descriptions are available in the customer documentations.


Security information
In order to protect technical infrastructures, systems, machines and networks against cyber threats, it is necessary to implement – and continuously maintain – a holistic, state-of-the-art IT security concept. Siemens’ products and solutions constitute one element of such a concept. For more information about cyber security, please visit
https://www.siemens.com/cybersecurity#Ouraspiration.
Rate entry
no rating
Requests and feedback
What do you want to do?
Note: The feedback always relates to the current entry / product. Your message will be forwarded to our technical editors working in the Online Support. In a few days, you will receive a response if your feedback requires one. If we have no further questions, you will not hear from us.