×
Siemens Industry Online Support
Siemens AG
Entry type: Product note Entry ID: 35125626, Entry date: 03/26/2009
(0)
Rate

SIMATIC PDM V6.0 + SP5 Released for Delivery

  • Entry
  • Associated product(s)

Service Pack 5 (SP5) is now available for SIMATIC PDM V6.0. New shipments of SIMATIC PDM V6.0 already include the SP5. You can order a free update to upgrade existing SIMATIC PDM V6.0, V6.0 + SP1, V6.0 + SP2, V6.0 + SP3 or V6.0 + SP4 software to V6.0 + SP5 via the online order form in entry ID 35125986. Alternatively you can also purchase the current SIMATIC PDM Demo V6.0 demonstration software with integrated SP5, order no. 6ES7 658-3GX06-0YC8, and use that to upgrade your SIMATIC PDM installations.

Reason for SP5

  • Accumulated qualitäty improvement measures since the release of Service Pack 4 for SIMATIC PDM V6.0
  • Adaptation to be able to use the HCF Catalog, Edition 03/2008
  • Optional deactivation of the automatic diagnostic update (reduces the time for uploading/downloading the parameters to/from the field device)
  • Support of the HART RIO SHC mode (fast HART communication):
    This functionality depends on the hardware. If the hardware supports this mode, communication with HART field devices is automatically accelerated.

Compatibility

Operating systems:

SIMATIC PDM V6.0 + SP5 will run under the following operating systems:

  • Microsoft Windows 2000 Professional SP3 or SP4
  • Microsoft Windows XP Professional SP2 or SP3
  • Microsoft Server 2003 SP2 or SP3 (only for operation on a SIMATIC PCS 7 Engineering Station)

Integration in SIMATIC PCS 7/SIMATIC STEP 7

SIMATIC PDM V6.0 + SP5 can be operated when integrated in the following configuration environments:

  • SIMATIC PCS 7 V6.1 + SP1, SP2 or SP3
  • SIMATIC PCS 7 V7.0 + SP1 or SP2
  • STEP 7 V5.2 + SP1
  • STEP 7 V5.3 + SP3
  • STEP7 V5.4 + SP3, SP4 or SP5

Use of the I&M profile of the PROFIBUS user organization and the related use of data set 255 for read and write jobs is only possible with:

  • SIMATIC PDM V6.0 + SP4 or SP5 for stand-alone operation
  • SIMATIC PDM V6.0 + SP4 or SP5, system integrated in SIMATIC PCS 7 V7.0 and higher
  • SIMATIC PDM V6.0 + SP4 or SP5, system integrated in SIMATIC STEP 7 V5.4 and higher

Please note that the included HART OPC Server of the HART Communication Foundation (HCF) has only been released for Windows NT and Windows 2000.

For more information please see the "Readme" files and the "What's new" file (all included in the file "Readme_PDM_V60_SP5.zip" at the end of this bulletin).

Scope of supply

The scope of supply of SIMATIC PDM V6.0 + SP5 includes the following CDs:

  • CD 1 with SIMATIC PDM V6.0 + SP5 software
  • CD 2 with the latest device library (Device Library 01/2009)

Integration and updating of devices

The device library of SIMATIC PDM V6.0 + SP5 (Device Library 01/2009) will integrate new devices and update the device descriptions of existing devices. The HART device library of the HART Communication Foundation (HCF), edition 03/2008, is also involved. More information on the devices listed in the device library of SIMATIC PDM V6.0 + SP5 (Device Library 01/2009) is available from the Internet pages of the device manufacturers, as well as from the language-dependent list of devices in the attached "List_of_Devices_1_2009.zip" file.

 List_of_Devices_1_2009.zip ( 15 KB )

The list below provides extracts of some newly included or updated devices. The table is not complete. For more information please see the device CDs or contact the manufacturer of the field devices.

 

Device Classification Manufacturer Communication
TTX200 v0.1 Sensors - temperaturee ABB HART
Cerabar M / PMx4x - Rev 1 Sensors - pressure Endress+Hauser HART
Cerabar S / PMx x3x - Rev 5 Sensors - pressure Endress+Hauser HART
Cerabar S / PMx x3x - Rev 7 Sensors - pressure Endress+Hauser HART
Cerabar S / PMx7x - Rev 1 Sensors - pressure Endress+Hauser HART
Cerabar S / PMx7x - Rev 20 Sensors - pressure Endress+Hauser HART
Cerabar S / PMx7x - Rev 21 Sensors - pressure Endress+Hauser HART
Deltabar S / xMD x3x - Rev 5 Sensors - pressure Endress+Hauser HART
Deltabar S / xMD x3x - Rev 7 Sensors - pressure Endress+Hauser HART
Deltabar S / xMP7x - Rev 1 Sensors - pressure Endress+Hauser HART
Deltabar S / xMP7x - Rev 20 Sensors - pressure Endress+Hauser HART
Deltabar S / xMP7x - Rev 21 Sensors - pressure Endress+Hauser HART
Deltapilot S / FMB70 - Rev 21 Sensors - level - hydrostatic Endress+Hauser HART
Deltapilot S / DB5x - Rev 2 Sensors - level - hydrostatic Endress+Hauser HART
Gammapilot M / FMG60 - Rev 1 Sensors - level - radiometric Endress+Hauser HART
Gammapilot M / FMG60 - Rev 2 Sensors - level - radiometric Endress+Hauser HART
Levelflex M / FMP4x - Rev 2 Sensors - level - echo Endress+Hauser HART
Levelflex M / FMP4x - Rev 4 Sensors - level - echo Endress+Hauser HART
Liquicap M / FMI5x - Rev 3 Sensors - level - capacitive Endress+Hauser HART
Micropilot II / FMR23x - Rev 2 Sensors - level - echo Endress+Hauser HART
Micropilot M / FMR24x-25x - Rev 5 Sensors - level - echo Endress+Hauser HART
Micropilot M / FMR250 - Rev 4 Sensors - level - echo Endress+Hauser HART
Micropilot M / FMR2xx - Rev 1+2 Sensors - level - echo Endress+Hauser HART
Micropilot M / FMR2xx - Rev 2 Sensors - level - echo Endress+Hauser HART
Micropilot M / FMR2xx - Rev 4 Sensors - level - echo Endress+Hauser HART
Promag 33/35 - Rev 2 Sensors - flow - electromagnetic Endress+Hauser HART
Promag 50 - Rev 1 V1.01.00 Sensors - flow - electromagnetic Endress+Hauser PROFIBUS PA
Promag 50 - Rev 6+7 Sensors - flow - electromagnetic Endress+Hauser HART
Promag 51 - Rev 6+7 Sensors - flow - electromagnetic Endress+Hauser HART
Promag 53 - Rev 1 V1.01.00 Sensors - flow - electromagnetic Endress+Hauser PROFIBUS PA
Promag 53 - Rev 1 V1.01.00 Sensors - flow - electromagnetic Endress+Hauser PROFIBUS DP
Promag 53 - Rev 6 Sensors - flow - electromagnetic Endress+Hauser HART
Promag 53 - Rev 1+2 Sensors - flow - electromagnetic Endress+Hauser HART
Promass 40 - Rev 8 Sensors - flow - Coriolis Endress+Hauser HART
Promass 80 - Rev 1 V1.01.00 Sensors - flow - Coriolis Endress+Hauser PROFIBUS PA
Promass 80 - Rev 8 Sensors - flow - Coriolis Endress+Hauser HART
Promass 83 - Rev 1 V1.01.00 Sensors - flow - Coriolis Endress+Hauser PROFIBUS DP
Promass 83 - Rev 1 V1.01.00 Sensors - flow - Coriolis Endress+Hauser PROFIBUS PA
Promass 83 - Rev 7+8 Sensors - flow - Coriolis Endress+Hauser HART
Promass 84 - Rev 8 Sensors - flow - Coriolis Endress+Hauser HART
Prosonic flow 90 - Rev 5 Sensors - flow - ultrasound Endress+Hauser HART
Prosonic flow 91 - Rev 1 Sensors - flow - ultrasound Endress+Hauser HART
Prosonic flow 93 - Rev 6 Sensors - flow - ultrasound Endress+Hauser HART
Prosonic S / FMU90 - Rev 1 Sensors - level - echo Endress+Hauser HART
Prowirl 70 - Rev 1 Sensors - flow - Vortex counter Endress+Hauser HART
Prowirl 72 - Rev 5 Sensors - flow - Vortex counter Endress+Hauser HART
Prowirl 73 - Rev 4 Sensors - flow - Vortex counter Endress+Hauser HART
Prowirl 77 - Rev 1 Sensors - flow - Vortex counter Endress+Hauser HART
TMT84 - Rev 1 (V01.00.XX) Sensors - temperature Endress+Hauser PROFIBUS PA
TMass 65 - Rev 1 Sensors - flow - thermal Endress+Hauser HART
iTEMP / TMT 122 - Rev 2 Sensors - temperature Endress+Hauser HART
iTEMP / TMT 162 - Rev 1+2 Sensors - temperature Endress+Hauser HART
iTEMP / TMT 182 - Rev 1+2 Sensors - temperature Endress+Hauser HART
IFC 090 Sensors - flow - electromagnetic KROHNE PROFIBUS PA
IFC 300 Sensors - flow - electromagnetic KROHNE HART
Stratos Pro Series - Stratos A211 X OXY Sensors - liquid analysis Knick HART
Stratos Pro Series - Stratos A211 X PH Sensors - liquid analysis Knick HART
Model 705 3.x - Rev 1+2 Sensors - level - echo Magnetrol PROFIBUS PA
ND9000P SW 1.51-1.80 Actuator - electropneumatic Metso Automation PROFIBUS PA
M420 Series - M420 O2 Sensors - liquid analysis Mettler Toledo HART
M420 Series - M420 PH Sensors - liquid analysis Mettler Toledo HART
373X-3 (Rev. 4+5+6) Actuator - electropneumatic SAMSON HART
373X-4 (PA-Profile 3.01) Actuator - electropneumatic SAMSON PROFIBUS PA
PAC3200 Power Monitoring Siemens PROFIBUS DP
SITRANS P DSIII.2 Sensors - pressure Siemens HART
SITRANS P300 Sensors - pressure Siemens HART
SITRANS TH300 Sensors - temperature Siemens HART
SITRANS TR300 Sensors - temperature Siemens HART
Hydro200 Sensors - level - echo Siemens Modbus
Multi100 Sensors - level - echo Siemens Modbus
Multi200 Sensors - level - echo Siemens Modbus

Installation

Important!

Before proceeding with the installation please read the information of the readme files. The "Readme" files together with the "What's new" file are included in the attached file "Readme_PDM_V60_SP5.zip".
Existing SIMATIC PDM V6.0 project data will be retained when you update to SP5.

 Readme_PDM_V60_SP5.zip ( 252 KB )

Security information
In order to protect technical infrastructures, systems, machines and networks against cyber threats, it is necessary to implement – and continuously maintain – a holistic, state-of-the-art IT security concept. Siemens’ products and solutions constitute one element of such a concept. For more information about cyber security, please visit
https://www.siemens.com/cybersecurity#Ouraspiration.
Rate entry
Requests and feedback
What do you want to do?
Note: The feedback always relates to the current entry / product. Your message will be forwarded to our technical editors working in the Online Support. In a few days, you will receive a response if your feedback requires one. If we have no further questions, you will not hear from us.