×
Siemens Industry Online Support
Siemens AG
Entry type: Application example Entry ID: 35214239, Entry date: 06/10/2009
(0)
Rate

User Logon to the Operator Panel via HMI-RFI

  • Entry
  • Associated product(s)

Problem
A plant with different plant parts is to be operated and parameterized with several operator panels.
Depending on whether a user operates or maintains the plant or performs setting work, different user authorizations are required.
Until now, the classic logon to the operator panel has been performed by manually entering the user name and the associated password.
This type of logon is to be supplemented by an RFID card that is read out by means of a card reader.

In addition, it is to be possible to use the RFID cards for the acquisition of materials management goods.

Solution:
This automation solution example comprises three operator stations.
The plant control level is mapped by an OPC client (using the example of MS Excel).
Card readers are connected to two of the three operator stations.
The operator panels and the MES level are connected to one another via Industrial Ethernet.

The figure below schematically shows the most important components of the solution.

Downloads

Content of Downloads

Download

Documentation 35214239_WinCCflexible_HMI-RFI_e.pdf ( 1938 KB )
Code 
WinCC flexible 2008 project (WinCC flexible 2008 SP1)
MES application (using the example of MS Excel)
35214239_HMI-RFI_CODE.zip ( 2651 KB )

 

History

Version

Modification

05/2009 First edition

Keywords
HMI RFID, OPC, OPC XML, SOAP, HTTP, Panel, WinCC flexible, RFID

Security information
In order to protect technical infrastructures, systems, machines and networks against cyber threats, it is necessary to implement – and continuously maintain – a holistic, state-of-the-art IT security concept. Siemens’ products and solutions constitute one element of such a concept. For more information about cyber security, please visit